Det ser ut som du kommer fra United States, men det aktuelle nettstedet du har valgt å besøke er Norway. Vil du endre nettsted?

Ja, takk! Nei, jeg vil være på det nåværende nettstedet

Enable high contrast mode

Controller waterproof/weatherproof rating

The S1-200 controller is built robustly. However, to ensure your equipment lasts as long as possible, install it in a place where it is protected from the elements.

The controller has an IP68 rating. While this means that the controller is well able to handle water, it is still advisable to keep it out of rain.

A good place to mount the controller is beneath the solar module.

Read this article for more information about mounting the controller:

Mounting the controller