It looks like you are coming from United States, but the current site you have selected to visit is Norway. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Plumbing and Heating Exhibition

4 oktober – 5 oktober, 2017  11:00 AM – 16:00 PM

Xylem will be showcasing a range of central heating pump solutions at this year’s PHEX plumbing and heating exhibition.

Xylem will be exhibiting a variety of pumps from its Lowara ecocirc range, designed specifically with the HVAC industry in mind.Visitors to the stand will be able to see the ecocirc BASIC, PRO, PREMIUM, XL and XL Plus models, as well as a variety of solutions from Xylem’s domestic and commercial building services portfolio – such as booster sets, drainage pumps and sewage products.

For those looking for a domestic hot water solution, the ecocirc BASIC circulator pump is ideal with its cost-saving capabilities and high operational efficiency. Thanks to its ECM technology and permanent magnet rotor, the ecocirc BASIC works to reduce unnecessary water consumption and electricity usage. In addition, the pumps are also installed with patented anti-blockage technology and an internal temperature sensor, which reduces the speed of the pump should overheating occur.