Det ser ut som du kommer fra United States, men det aktuelle nettstedet du har valgt å besøke er Norway. Vil du endre nettsted?

Ja, takk! Nei, jeg vil være på det nåværende nettstedet

Enable high contrast mode

Installing the pump in a well

Follow these steps to install the S1–200 in a well.

  1. Make sure the controller is turned off and all cables are connected
  2. Make sure the hose is connected tightly with the hose clamp
  3. Attach a safety rope to the pump (see video below)
  4. Slowly lower the pump into the well
  5. Attach the rope to a pole or similar robust structure next to the well

Further reading

Connecting a hose to your pump