Wygląda na to, że pochodzisz z United States, jednak witryna, którą zdecydowałeś się odwiedzić, to Poland. Czy chcesz zmienić witryny?
Tak, poproszę. Nie. Chcę zostać na aktualnie wyświetlanej witrynie.
Xylem’s
The Panama Canal Expansion Program is scheduled for completion in the
second quarter of 2016. It creates a new traffic lane and builds two new
lock complexes, one on the
"We are honored to work with the
This is the second project that the ACP has awarded to Xylem under the Panama Canal Expansion Program. Earlier this year, Xylem supplied 64 Flygt mixers to prevent the formation of corrosive deposits on the rolling gates during installation.
To support the dewatering project, Xylem installed 15 Godwin
diesel-driven pumps, deployed from the U.S. In June, these pumps
transported up to 122 million gallons of water per day (MGD) from the
Xylem is providing turnkey services and equipment for the project, with
Xylem’s highly-skilled engineers designing and installing the system,
which also includes 13,500 feet (more than 2.5 miles) of 18-inch
high-density polyethylene pipeline (HDPE) to transfer the massive
amounts of water. Xylem is also supervising the performance of the 15
The third set of basin locks includes reuse basins that will save water and also improve the Panama Canal’s efficiency, using seven percent less water compared with the amount currently used by the existing locks. In addition, in each transit operation, 60 percent of the water will be recycled.
About Xylem
Xylem (XYL) is a leading global water technology provider, enabling
customers to transport, treat, test and efficiently use water in public
utility, residential and commercial building services, industrial and
agricultural settings. The company does business in more than 150
countries through a number of market-leading product brands, and its
people bring broad applications expertise with a strong focus on finding
local solutions to the world’s most challenging water and wastewater
problems. Xylem is headquartered in
The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all -- that which occurs in nature. For more information, please visit www.xyleminc.com
View source version on businesswire.com: http://www.businesswire.com/news/home/20150729006054/en/
Source:
Xylem
Inc.
David Callaghan, +353-87-938-8880
David.Callaghan@edelman.com
or
Investors
Phil
DeSousa, +1-914-323-5930
Phil.Desousa@xyleminc.com