Úgy néz ki, az országa United States, de az aktuálisan kiválasztott weboldal Hungary. Kíván oldalt váltani?

Igen, kérem. Nem. Maradok a jelenlegi oldalon.

Enable high contrast mode

Installing the pump in a well

Follow these steps to install the S1–200 in a well.

  1. Make sure the controller is turned off and all cables are connected
  2. Make sure the hose is connected tightly with the hose clamp
  3. Attach a safety rope to the pump (see video below)
  4. Slowly lower the pump into the well
  5. Attach the rope to a pole or similar robust structure next to the well

Further reading

Connecting a hose to your pump