Keresési eredmények
-
Reliable Water Management for Central Sterilization
St. Luke’s Hospital is a leading health care provider in southeastern Massachusetts with a wide range of medical and surgical services. Specialized areas include neurosurgery, cardiology, children’s health services, and orthopedic and general surgery.
-
Remote monitoring & controls for unmanned reliability
Xylem was tasked with designing a seep collection system to collect water from a low volume seep through the wall of a decommissioned fly ash pond. The sump was located in an active river floodplain that flooded with as little as 1-2 inches of rain, so the customer needed an automatic shutdown when the river covered the sump.
-
Remote Pumping Solution helps Mine Operators Reach New Depths in Harsh Environment
A customer in Perú needed to drain water as its large open-pit mine operation reached as deep as 1,200 ft (365 m) below the surface. The discovery of more copper in the mine, and an expected excess of water during rainy summer months also prompted the company to act. They sought a remote solution for monitoring and controlling their pumping system, particularly as routing electrical power became more difficult the deeper they dug....
-
Rented pump system supports major Scottish Water refurbishment
A temporary pumping system enabled improvements to be completed at a major Scottish Water pumping station, ensuring uninterrupted operation throughout a 10-month project -
Risks associated with the use of dispense gases in a food and beverage service establishment
A dispense gas is simply a pressurized gas used for dispensing drinks. The gas of choice is typically carbon dioxide (CO2), especially for carbonated drinks such as soda and beer. Carbon dioxide is commonly employed in the food service environment in a variety of equipment systems such as carbonation, refrigeration, and....
-
-
-
Saint-Gobain Containers, Inc. reduces DI water operation cost
Saint-Gobain Containers, Inc., of Milford, Massachusetts was using separate bed and mixed bed service deionizers to purify water for manufacturing glass containers used in the U.S. wine, beer, beverage, spirits and food industries.
-
San Diego plant cuts THM levels in half
The 34 MGD Otay Water Treatment Plant in San Diego, California serves a population of approx. 200,000. The plant receives raw water from two sources - imported water from the Colorado River and runoff from three local reservoirs.
-
-
Sazerac Northwest Ordinance Distilling (NOD) plant upgrades to sustainable anaerobic membrane bioreactor (AnMBR) system
The cost of hauling wastewater caused Sazerac Distilling to upgrade its wastewater treatment system to a sustainable anaerobic membrane bioreactor (AnMBR) system by Xylem. -
SCV Water Agency selects Xylem vessels & media for PFAS removal
Santa Clarita is located about 35 miles north of Los Angeles. The Santa Clarita Valley Water Agency (SCV Water) services nearly 74,000 customers and obtains about 50% of its drinking water through local groundwater aquifers. Positioned behind the William S. Hart community baseball and softball fields three two-vessel systems have been installed to remove PFAS from drinking water.
-
Secure in-field firmware updates to support more resilient connected products
EU Cyber Resilience Act: Manufacturers must report vulnerabilities from Sept 2026, with full compliance required by Dec 2027 -
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
-
Soil and groundwater remediation
Soil and groundwater remediation projects often call for treatment of groundwater, soil vapor extraction condensate, soil vapor and other liquid and vapor streams for removal of volatile and semi volatile organic compounds. Xylem's Carbonair has provided thousands of STAT Low Profile Air Strippers, liquid phase and vapor phase carbon vessels for remediation systems over our 30 plus years in business.
-
-
Southern California water utility consults Xylem for disinfection of potable water
Located in Southern California, this water utility uses wells to store water. These same wells are also used for fire protection. which is especially critical during the summer months. The supply covers about 10,000 customer connections with chloraminated water for residual disinfection, with chlorine and ammonia boosting in various locations.
-
Specification Tips to Maximize Heat Transfer: Shell and Tube
Heat exchangers are widely used in various industries including chemical, oil & gas, power generation, food & beverage, HVAC & refrigeration, pulp & paper to name a few, and are expecting strong growth over the coming years driven in part by a rising focus on environmental impact and improving efficiency standards.
-
-
Stadtwerke Trier: AI-aided energy optimization for daily energy balancing
Xylem Vue helped Stadtwerke Trier optimize renewable energy use in its drinking water network, achieving 90% self-consumption. -
Sugar company finds sweet solution for odor control
The sugar company produces approximately 4,500,000 cwt. of sugar per year, resulting in high-strength wastewater that creates odors, especially during the company’s peak season in the spring and summer. The company was using a series of basins, such as ponds and ditches, to cool, equalize, settle, and digest the organic wastewater.
-
Supervision of pumping stations in Vlaardingen is highly effective
In the municipality of Vlaardingen, rainwater and wastewater are processed by more than seventy pumping stations, six of which are large, dry-installed main pumping stations and a large number of subsidiary and mini-pumping stations. Supervision is the responsibility of Xylem, which means that the Vlaardingen maintenance department receives a weekly overview of all relevant events.
-