It looks like you are coming from United States, but the current site you have selected to visit is Hungary. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode
Flexible Impeller Replacement Troubleshooting Guide

Flexible Impeller Replacement Troubleshooting Guide

This guide will cover various issues experienced with flexible impellers based on symptoms, what causes the issue, and the remedy for each scenario. 

Troubleshooting 1

Symptoms

  • End faces hard and either polished or cracked, like carbon
  • Some or all blades completely missing

 

Cause

  • Dry running; lack of water in pump
  • Temporary suction blockage
  • Leaking suction plumbing

Remedy

  • Do not run pump for more than 20 seconds without liquid
  • Install a liquid sensor/temperature alarm
  • Check suction plumbing, strainers, and through hull fittings for blockages and leakage
  • Arrange discharge plumbing to trap liquid in the pump

Troubleshooting 2

Symptoms

  • Pieces missing from the middle of blade tips
  • Blade edges are hollowed out
  • Pitting is evident on cam and the inside of pump ports, and on ends of impeller

Cause

  • Cavitation, i.e., too much vacuum on inlet is causing water to boil inside pump

Remedy

  • Reduce pump speed
  • Increase inlet plumbing diameter
  • Reduce inlet plumbing length and remove unnecessary restrictions
  • Reduce cam thickness

Troubleshooting 3

Symptoms

  • Worn blade tips, cam imprint on edges
  • Worn end faces
  • Worn impeller drive and shaft wear

Cause

  • Abrasive wear from fluid in pump
  • Heat exchanger/cooler blockage
  • High discharge pressure

Remedy

  • Check discharge plumbing for partial blockages
  • Increase discharge pipe diameter

Troubleshooting 4

Symptoms

  • Impeller appears to have swollen
  • Blades appear wider than impeller hub
  • Rubber may feel sticky

Cause

  • Chemical attack, more common with oily bilge water or diesel transfer

Remedy

  • Ensure impeller is rinsed after use
  • Remove impeller when not in use
  • Remove impeller for long-term storage

Troubleshooting 5

Symptoms

  • Blades have some or severe permanent set

Cause

  • Normal use of impeller
  • Long-term storage in pump
  • Normal end of impeller life

Remedy

  • Refit impeller to rotate in opposite direction
  • Remove impeller for long-term storage
  • Replace impeller

Troubleshooting 6

Symptoms

  • Blades cracked about halfway up the length
  • Some blades missing
  • Reduced flow

Cause

  • Normal end of impeller life
  • High discharge pressure

Remedy

  • Replace impeller; check for impeller pieces in discharge plumbing
  • Reduce outlet restrictions or increase outlet plumbing diameter