Zoekresultaten
-
Ion exchange services remove groundwater contaminants
California Water Service Company had acquired another water company with approximately 100 connections, in Porterville, California, located in a remote agricultural area of the Central Valley. Their annual well testing had shown levels of nitrate at or near the Maximum Contamination Level (MCL) of 45 ppm and perchlorate was found in the groundwater at levels above the Public Health Goal (PHG) of 10 ppb. A treatment system was needed to remove both these contaminants to ensure quality potable water for the local community.
-
-
Kraft Foods achieves excellent nutrient removals
Due to an expansion in potato chip production, the snack food plant required additional wastewater treatment capacity. It needed to be able to meet strict discharge limits for biochemical oxygen demand (BOD), total suspended solids (TSS), ammonia nitrogen (NH3-N), total nitrogen (TN), and total phosphorus (TP) regulations.
-
Landfill leachate treatment system significantly reduces operations cost
The South Central Counties Solid Waste Agency, located in Hopewell, Pennsylvania needed a cost effective, on-site treatment system to treat 12,500 gpd of leachate and allow for future expansion.
-
-
Logan Township, NJ expands water reclamation facility
Situated on the banks of the Delaware River, Logan Township, New Jersey has a long history of caring for its watershed and natural environment. In the early 70s, the town designed what has been described as “the nation’s first ecologically planned industrial complex,” Pureland Industrial Complex.
-
Bilge Water Pumping
Bilge water pumping solutions remove unwanted water from boat bilges using electric, manual, and engine-driven pumps designed to support reliable bilge water...
-
Biofuel
Biofuels are a growing market, not only for vehicle propulsion, but for other uses such as heating and cooling. Our solutions are used across agriculture and...
-
Boat Washdown
Whether you're rinsing saltwater and bird droppings off the deck or mud off an anchor, an onboard washdown system provides a convenient means to hose down the...
-
Boiler Feedwater Treatment
Improve boiler feedwater treatment with systems that remove suspended solids, dissolved minerals, and gases to prevent scaling and fouling, enhance efficiency,...
-
Central Sterile Processing
Water quality is an important consideration in all stages of medical device reprocessing with the primary objective of ensuring that surgical instruments and...
-
Coal Ash
Next-generation water management in coal ash starts with a holistic view of how your operation can run more reliably, safely, and productively. Whether you’re...
-
Combined Sewage & Stormwater Handling
Combined sewers cause serious water pollution problems during combined sewer overflow (CSO) events. This occurs when combined sewage and surface runoff flows...
-
Deep Well Dewatering
Deep well dewatering is used for ground preparation where deep excavations, beyond the maximum limits for wellpoint systems, are necessary like tunnels, dams,...
-
Diesel Transfer
If you've ever run out of fuel while out on the water, you know how vital a diesel transfer pump can be. Not only can it help you transfer diesel between aft...
-
Disinfection Byproducts Control
Disinfectants can react with natural materials in source water to form disinfectant byproducts. The most common disinfectant byproducts are Trihalomethanes...
-
Disinfection, Safety and Sanitation for the Food & Beverage Industry
Waterborne microorganisms can affect flavor, color, odor, and shelf life of soft drinks, bottled water and a wide variety of food products. It is critical that...
-
Dust Suppression
Control dust in mining operations using pumping systems that optimize water and energy use while improving safety, equipment performance, and environmental...
-
Electrochlorination for Offshore HVDC Transmission Systems
Offshore wind is becoming a leading source of renewable energy and it is critical that High Voltage Direct Current (HVDC) transmission system meet performance...
-
Flue Gas Desulfurization (FGD) Wastewater
Fossil-fuel power plants emit exhaust that includes sulfur dioxide —among other substances considered harmful to the natural environment—that must be treated...
-
Micropollutants, Taste & Odor Control
Many municipalities seek to control micropollutant, taste and odor issues to minimize consumer complaints, meet aesthetic standards, or to comply with...
-
Nitrogen removal in wastewater treatment
Nitrogen removal is a critical part of wastewater treatment. When excess nitrogen is discharged to receiving water, it can contribute to eutrophication,... -
PFAS Remediation for Construction Dewatering
Construction site water caused by excavation must be pumped away from the site and treated properly. This remediation process typically requires the removal of...
-
Phosphorus Removal and Recovery
Wastewater typically contains a large amount of nutrients - particularly phosphorus - that can pose a harmful threat to infrastructure and the environment,...