Het lijkt erop dat u van United States komt, maar de huidige website die u wilt bezoeken is Netherlands. Wilt u van website wisselen?

Ja, graag. Nee. Ik wil op de huidige website blijven.

Saving Energy at Wastewater Treatment Plants with Ammonia Control

Wastewater Treatment Plants (WWTPs) play a key role in protecting natural water bodies, however they are also one of the largest energy consumers in most countries. Many investigations have been applied to energy-saving in WWTPs but the transformation of aeration control systems is the most efficent and economical. Based on studies conducted in Japan, energy-savings of aproximately 20% can be realized by using an Ammonia control system as an alternative to the commonly used Dissolved Oxygen (DO) control system.

In this webinar WTW product specialist Dr. Tao Su will discuss:

  • What we can do to save energy in WWTPs
  • Current DO control system of aeration
  • The pricicple of energy-saving by ammonia control system
  • Successful cases that utilize ammonia control system

Meet the Presenter

Tao-Su-Circle-Blue.pngDr. Tao Su, Xylem Product Manager.
Responsible for product sales and promotion of WTW online products throughout North Asia. Dr. Tao has been with Xylem for 3 years and has a PhD in Environmental Sciences from the University of Tokyo.

 

 

Original Webinar Broadcast Date:

June 17th, 2021