Het lijkt erop dat u van United States komt, maar de huidige website die u wilt bezoeken is Netherlands. Wilt u van website wisselen?

Ja, graag. Nee. Ik wil op de huidige website blijven.

Hoog contrast modus inschakelen

Casestudies

Casestudies

  • Hot to cold, from start to finish

    Our technology plays a key part in managing water delivery through all elements of the HVAC cycle. The products can be categorised into those best suited to commercial applications and those for domestic and residential use.
  • Lowara Pumps help support a unique nickel extraction project

    The Thakadu Nickel Purification Plant utilises a process called Nickel Crystallization. A crude nickel sulfate stream is pumped to the purification plant, where it is heated and evaporated into a vacuum, forming nickel sulfate crystals for harvesting.
  • Healthy Recovery

    Lowara, through its local distributor Efstratiadis SA, collaborated closely with the internal construction team headed by Dr. Papavasilopoulos Fotios, Managing Director of Olympion Clinic, in order to choose the best re-circulation and pumping solutions.
  • Better effluent quality with the fourth wastewater treatment stage at Aachen-Soers

    In search for the best wastewater treatment process in terms of removal of microbiological contaminants and the abatement of bromate discharge, RWTH Aachen University, along with the other environmental institutions, launched a research project and partnered with Xylem to test the effects of wastewater ozonation on water quality and its ecosystem.
  • Future-proof water supply for the Waldviertel, Austria

    EVN Wasser GmbH, the largest water supplier in Lower Austria, implemented a groundbreaking infrastructure project between 2020 and 2025: the new construction of the drinking water Waldviertel pipeline. This 60-kilometre-long main supply pipeline from the Grunddorf/Donaudorf fountain field to Zwettl secures the future supply of high-quality drinking water to around 120,000 inhabitants – an investment in quality of life and future security for an entire region.
  • World’s Tallest Building

    Ahmed Ramadhan Juma (ARJ) is supplying 6 water transfer sets (11KW-200KW) and 7 water booster sets (4KW-37KW) utilising vertical and horizontal multistage pumps. The water booster sets are fitted with “Hydrovar”, a bespoke variable speed drive (VSD) designed for pumping applications.