Sembra che tu risieda in United States ma il sito che hai attualmente selezionato per visitarci รจ Italy. Vuoi cambiare sito?

Si, grazie! No desidero rimanere in questo sito

Enable high contrast mode

High Efficiency Filtration Reduces Turbidity & Maintenance Costs

Viewing of otter habitat greatly improved through installation of Vortisand® media filter at the Montreal Zoo

The Ecomuseum Zoo is home to the most impressive ambassadors of Quebec’s wildlife. All residents of the Ecomuseum Zoo are there for a special reason: orphaned, injured or born under professional human care, each of them could not return to the wild. Hence, they have found a forever home at the zoo.

The $1.4 million 6,000 square foot river otter habitat, first of its kind in Canada, is made up of vast land, river banks and a 250,000 litre (66,000 gallon) water basin; includes two port holes, an underwater tunnel and a 15 meter (50 foot) viewing window. In order to improve water clarity, a high efficiency submicron performance filtration system was required to fit in a 3 meter by 4 meter (10 foot by 14 foot) mechanical room.

With the need to filter contaminants and fine particles, engineering consultants had specified Vortisand cross-flow filtration technology as the go to side stream filtration system.

Challenge

The footprint of the mechanical room presented itself as one of the first challenges the Ecomuseum Zoo was faced with. With only a portion of the mechanical room space being dedicated to the water filtration system, our team of application engineers were mandated to design a customized configuration. The natural outdoor environment of the habitat posed a second challenge for the Ecomuseum Zoo and engineering consultants. Over time the water basin acts as an air scrubber, absorbing airborne contaminants and debris as they brush along the surface of the water. These contaminants can buildup and create a film on various types of hard surfaces, potentially covering the viewing window and other surfaces found within the otter habitat. The airborne contaminants and debris also increase the risk of experiencing higher levels of water turbidity. Such high levels of turbidity will result in reduced water clarity, further limiting the learning experience for Ecomuseum Zoo visitors. Routine water basin cleaning would be costly, and the use of harmful chemicals are prohibited; ultimately requiring the removal of the fine particles before they have the chance of creating a concern. The Vortisand system was required to handle various types of contaminants and fine particulates, while yielding minimal maintenance and operational related costs.

Solution

Thanks to its compact design, the Vortisand H2F® system was installed within the current parameters of the maintenance room. Its submicron filtration performance and high efficiency capabilities helped remove the fine particles that would otherwise make it impossible for visitors to see the otters through the viewing glass, portholes and underwater tunnel. Most importantly, the Vortisand® system made it possible for the otters to go about their daily activities comfortably. With minimal maintenance and manual intervention required, the Ecomuseum Zoo employees were able to focus on nurturing and growing their family.

Results

Upon start up a particle analysis test was conducted, showing that particles of 5 micron and less in size made up the vast majority of the particles within the river otter aquarium. The Vortisand system delivered 94% removal of particles less than 5 micron in size.

"Every effort is made to provide an exceptional level of care. Here at the Ecomuseum Zoo, we make animal welfare our number one priority, and this habitat is a faithful reflection of that choice. Nothing has been neglected to ensure that the River Otters in our care have a safe, soothing and stimulating environment. We are deeply satisfied with the work achieved by Vortisand systems. Being able to work with such a high level product means a lot for our team’s efficiency and our animals’ well-being, two of our main concerns."
David Rodrigue, Executive Director of the Ecomuseum Zoo