Resultados da pesquisa
-
-
-
AWWA ACE24
At ACE, we come together to discuss and plan for the serious issues that will transform the future of water. Together, we will make an impact that will determine the trajectory of our planet. Attend ACE and collectively, we will transform the future of water.
-
-
-
-
-
-
-
-
-
Cookies
This website makes use of cookies to ensure the best experience for all of our visitors, we have listed and categories the different cookies that we make use...
-
-
Energy Savings Calculator
Energy saving potential Significant opportunities exist to reduce pumping system energy consumption through smart hydraulic system design, retrofitting to...
-
Help
Understanding solar pumps S1-200 Application Types Flow and head of an S1-200 pump system Suitable water temperature Tolerable salt and sand content Required...
-
How to clean the remote tank switch
Like the S1-200 pump, the Remote Tank Switch should not be used in extremely dirty, sandy or muddy water. If the pump is operated with liquid under normal...
-
Overheating controller
The S1-200 controller is built robustly. However, to ensure your equipment lasts as long as possible, install it in a place where it is protected from the...
-
Cleaning the pump end
Your LORENTZ pump is a helical rotor pump, which means it is able to handle some degree of dirt. You should not run it in very dirty, sandy or even muddy...
-
The pump does not start or delivers too little water
If your pump does not start, or delivers less water than expected, please check the following: Solar Module Check whether all plugs are connected correctly...
-
Setting the daily water amount
The S-Connect App has a function called "Daily amount" that can be activated when needed. This function allows you to set the maximum limit of water pumped per...
-
Managing sensor inputs and accessories with the S-Connect app
If you need to deactivate any sensor inputs of your LORENTZ pump system, this is easy with the S-Connect app. go to " Settings " and then " Advanced Settings...
-
Setting a timer for the pump
How to set a timer for the pump To set a timer, go to " Settings ". Activate the " Timer " function and select the type of timer needed. You can choose between...
-
Wall mounting the controller
The S1-200 controller can be mounted to a wall or other flat surface. You will need 2 x screws that are appropriate for material your are fixing to. The screws...
-
Installing the pump in a well
Follow these steps to install the S1–200 in a well. Make sure the controller is turned off and all cables are connected Make sure the hose is connected tightly...