Bem-vindo(a) à Making Waves, onde irá encontrar histórias sobre a água e a Xylem, uma empresa global de tecnologia da água com uma missão de resolver os problemas da água.
Escolha artigos e publicações de blog da nossa seleção de tópicos populares abaixo, leia uma das histórias das escolhas do editor, deslize pelo Feed de Notícias ou escolha Filtrar Por na barra de navegação superior para ter acesso a todas histórias e tópicos da Making Waves. Subscreva a nossa Newsletter mensal para estar atualizado sobre o maravilhoso mundo da água.
Notícias sobre a Água Sustentabilidade Inovação Zero Emissões Líquidas Analítica
Escolhas do Editor
Todas as publicações em Making Waves
3 Ways Xylem Customers are Solving Non-Revenue Water
Non-revenue water – or treated water that is unbilled or “lost” due to leaking infrastructure, inaccurate meters or theft – is a major issue facing water...
Xylem Commercial Accelerator Spotlight: Speeding Technology Adoption Across Diverse Landscapes
Innovation is creating unprecedented and practical ways to solve global water threats like water scarcity, water affordability, and infrastructure resilience...
South Coast Mariculture wanted to better understand the water quality conditions of their mussel farms in Jervis Bay, located in New South Wales, Australia....
Mina Guli speaks up on the need to protect the source
A Q&A with water advocate and ultramarathon runner, Mina Guli Empowering people to protect our water sources is a vital quest that unites Xylem Watermark and...
The Solving Water podcast, featuring host Amanda Holloway, Demand Generation Manager at Xylem, wades into the trending topics, technology and behind-the-scenes...
By recirculating and treating shower water in real time, the innovative LOOP shower system reduces water consumption by up to 80% and energy usage by 70%. When...