Bem-vindo(a) à Making Waves, onde irá encontrar histórias sobre a água e a Xylem, uma empresa global de tecnologia da água com uma missão de resolver os problemas da água.
Escolha artigos e publicações de blog da nossa seleção de tópicos populares abaixo, leia uma das histórias das escolhas do editor, deslize pelo Feed de Notícias ou escolha Filtrar Por na barra de navegação superior para ter acesso a todas histórias e tópicos da Making Waves. Subscreva a nossa Newsletter mensal para estar atualizado sobre o maravilhoso mundo da água.
Notícias sobre a Água Sustentabilidade Inovação Zero Emissões Líquidas Analítica
Escolhas do Editor
All Posts in Water Utilities
Rural North Texas community cuts non-revenue water by 42% with pipeline leak detection technology
In the rural city of Iowa Park, Texas, the Cypress Water Transmission Line serves as a community backbone – delivering drinking water to 6,000 residents and...
More than 90% of global disasters are linked to water, and their impacts are growing. In 2024, floods, storms and droughts caused over $550 billion in economic...
Flowing through the heart of Knoxville, Tennessee, Beaver Creek is more than just a local waterway – it’s a 303(d) listed stream, meaning it’s been flagged by...
Athens and Los Angeles. These two cities are thousands of kilometers apart, operating in vastly different contexts but pointing in the same direction....
The small town of Clifton, Colorado, is known for its outdoor recreational activities, proximity to local vineyards, and stunning views of the Colorado River....
On Catalonia’s sun-drenched coast, the utility Consorci d’Aigües de Tarragona (CAT) faces prolonged droughts and unpredictable water quality. As the region’s...