It looks like you are coming from United States, but the current site you have selected to visit is Portugal. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Resultados da pesquisa

Resultados da pesquisa

  • Waste Management for Agriculture

    Manure handling is an important application in animal breeding where water plays an essential role in effective waste management. Farmers need reliable and...
  • Wastewater Disinfection

    Ensuring that water remains clean and free from dangerous pathogens is critical for safeguarding public health and the environment. Contaminated water can pose...
  • Water for Injection (WFI)

    Water for Injection (WFI) is a water quality standard defined by pharmacopeial groups worldwide. WFI is used for the most critical pharmaceutical products and...
  • Water Reuse for Microelectronics

    Enable sustainable water reuse in microelectronics manufacturing by identifying wastewater streams and using advanced treatment technologies to improve water...
  • Cookies

    This website makes use of cookies to ensure the best experience for all of our visitors, we have listed and categories the different cookies that we make use...
  • Energy Savings Calculator

    Energy saving potential Significant opportunities exist to reduce pumping system energy consumption through smart hydraulic system design, retrofitting to...
  • Help

    Understanding solar pumps S1-200 Application Types Flow and head of an S1-200 pump system Suitable water temperature Tolerable salt and sand content Required...
  • How to clean the remote tank switch

    Like the S1-200 pump, the Remote Tank Switch should not be used in extremely dirty, sandy or muddy water. If the pump is operated with liquid under normal...
  • Overheating controller

    The S1-200 controller is built robustly. However, to ensure your equipment lasts as long as possible, install it in a place where it is protected from the...
  • Cleaning the pump end

    Your LORENTZ pump is a helical rotor pump, which means it is able to handle some degree of dirt. You should not run it in very dirty, sandy or even muddy...
  • Setting the daily water amount

    The S-Connect App has a function called "Daily amount" that can be activated when needed. This function allows you to set the maximum limit of water pumped per...
  • Setting a timer for the pump

    How to set a timer for the pump To set a timer, go to " Settings ". Activate the " Timer " function and select the type of timer needed. You can choose between...
  • Wall mounting the controller

    The S1-200 controller can be mounted to a wall or other flat surface. You will need 2 x screws that are appropriate for material your are fixing to. The screws...
  • Installing the pump in a well

    Follow these steps to install the S1–200 in a well. Make sure the controller is turned off and all cables are connected Make sure the hose is connected tightly...
  • Hose sizes compatible with the pump

    The S1-200 is designed to easily connect to standard 1" hoses. This is equivalent to an inner diameter of 25 mm. Other hose sizes can be attached via an...

Create Wishlist

Add to wishlists
Select one or more wishlists.

Item successfully added to wishlist.

Item successfully added to new wishlist.
Item successfully added to existing wishlist.