Resultados da pesquisa
-
Exporting pump data in the S-Connect app
Your pump system stores data about solar power, water flow, motor speed, errors and many other things. The data can be accessed in the app while connected to...
-
Reducing the amount of water pumped / Adjusting motor speed
If the water flow is too high for your application, there is an easy way to limit the flow with the S-Connect app. To lower the water flow you simply reduce...
-
Using the S-Connect app with your pump system
LORENTZ S-Connect turns any Android Smartphone or tablet into a management and configuration tool for S-Line LORENTZ pumps. You can easily configure your pump...
-
Checking how much water has been pumped
You can easily check the amount of water pumped in the dashboard of the S-Connect app. Open the app Connect to the pump controller via Bluetooth® Check the...
-
Meaning of LED sequences
The LED sequences on your controller give you information about your pump system. In the video below you find the sequences and their corresponding icons in...
-
How to switch on the S1-200 pump system
The S1-200 ON / OFF switch is located in the top right next to the LEDs. To switch on the system switch to on ( 1 ). The LED will go from flashing green...
-
Using the pump in a horizontal position
The S1-200 can be used in horizontal position as long as it is protected from dirt or mud. Pumping water with higher particle concentrations than indicated...
-
Downloading the S-Connect app
Download the Xylem S-Connect app for use with your S1 system. Xylem S-Connect is available for Android or IOS devices. Xylem S-Connect in Google PlayStore...
-
Controller waterproof/weatherproof rating
The S1-200 controller is built robustly. However, to ensure your equipment lasts as long as possible, install it in a place where it is protected from the...
-
Connecting cable extensions for motor and accessories cables
Motor and accessory cable extensions are available for purchase. They provide an easy plug and play solution for extending cable length. Because of power...
-
Connecting a hose to your pump
The S1-200 pump is designed to be used with a 25 mm (1.0 in) hose. Please refer to this video to learn how to attach a hose to your pump: Further reading Hose...
-
Activation of accessories without the S-Connect application
Activation of dry run protection accessory without S-Connect App In case you do not have a smartphone at hand and wish to activate the dry-running protection...
-
Mounting the controller
There are a few things to keep in mind when mounting the controller: it should not be in sun a shaded place is best it should be protected from rain if...
-
Function and use of tank full switch
With a float switch, the pump works autonomously, saving you time and effort. The tank full switch is a useful accessory to use with tanks. A float switch...
-
Function and use of remote tank switch
With the Remote Tank Switch accessory you can automatically control filling of remote tanks. The Remote Tank Switch is used where the tank that is being filled...
-
Well size requirements
The S1-200 is a small submersible pump that can be used in a range of applications. If you are installing your pump in a well, it needs to have a 100 mm (4.0...
-
Connecting PV modules in series and parallel
Understanding the connection of PV modules in series and parallel is essential not only for a correct installation and performance of the pump, but also to...
-
Flow and head of a S1-200 pump system
The S1-200 offers great flexibility to ensure maximum efficiency in every application. For this reason we designed three different pump ends: HR07, HR14 and...
-
S1-200 Application Types
Table of Contents S1-200 used to irrigate a field with a hose S1-200 used to irrigate a field using sprinklers S1-200 used in drip irrigation S1-200 used to...
-
3 Ways to Protect Your PCCP Now and into the Future
Obtaining actionable condition insights helps utilities prevent sudden and high-consequence PCCP failures. But is your asset management plan equipped to...
-
A Day in the Life: PipeDiver Inspection with Pressurized Insertion & Extraction
Join me onsite for a raw water pipeline inspection with the PipeDiver ® platform. I recorded this video in the field to show how we use specialized standpipes...
-
Asset Management Begins With Leak Detection
A leak represents not only water loss, but can indicate the potential for pipeline failure. How proactive utilities are taking the gamble out of finding leaks...
-
Beyond Water Loss: How Leak Detection Benefits Pipeline Management
World Water Loss Day on Dec. 4 brings awareness to the fact that billions of gallons of treated drinking water are lost from supply networks every day. 1 Water...
-
Channeling Utility Challenges into Technology Innovation
An Interview with Brian Youngpyo Jo, Senior Manager of Product Engineering Innovation often comes from pain, says Brian Youngpyo Jo, Senior Manager of Product...