Resultados da pesquisa
-
City of Kaufbeuren: increasing energy and resource efficiency through AI-based process control
In the face of climate change and cost and supply uncertainties, cities and municipalities must operate their plants and processes as efficiently and sustainably as possible. In this context, the town of Kaufbeuren recognized significant potential for energy optimization at its wastewater treatment plant.
-
City of Mesa pinpoints critical leak, avoiding costly delays
Discover how the City of Mesa, Arizona, used Xylem's SmartBall® technology to pinpoint a hard-to-find pipeline leak, safeguarding infrastructure and avoiding costly delays to a transportation project. -
-
-
Clayton County, Georgia reduces apparent water loss & identifies one million in recoverable revenue
Clayton County Water Authority (CCWA) is a good example of a utility that doesn’t let a confined geographical footprint stop it from thinking outside the box. As one of Georgia’s smallest counties in terms of land size area (only 143 square miles), its location near the top of a regional watershed means it has little area to gather precipitation into streams and rivers.
-
Complex Discharge Line Bypass at National Brewery Keeps Operations Online
A national beer brewery in Georgia needed to address deterioration and replacement of some of the drain pipes running from their fermentation tanks. For this to be classified as a successful repair and replacement effort, it needed to be achieved while keeping 25,000 barrels of beer a day flowing and simultaneously maximizing plant uptime and profitability.
-
Confectionery manufacturer eliminates sludge dewatering
The client makes several types of confectionery products at its facility. Its wastewater was being treated in a dissolved air flotation (DAF) system, followed by a dual-tank sequencing batch reactor (SBR) activated sludge system.
-
Cover helps community control odors from wastewater treatment
When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.
-
Delivering cost-effective process monitoring for the welding industry
Discover how Sentec engineered a compact, non-intrusive smart connector to digitally transform welding operations. From non-contact wire speed sensing to seamless Bluetooth integration, this case study highlights a scalable solution built for regulation, reliability and industry-wide adoption. -
Electric Generating Station Maximizes Plant Efficiency
Xcel Energy is a leading provider of electricity and natural gas to customers in the Midwestern US. As part of their expansion plans for the Comanche Station, a coal-fired electric generating station located in Pueblo, CO, Xcel Energy contacted Evoqua Water Technologies to explore cost effective solutions for their water treatment needs.
-
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
EMASA: improving water efficiency through smart water balance analysis
EMASA (Empresa Municipal Aguas de Málaga S.A.) is the Malaga City Council’s public utility which has been in charge of managing the entire urban water cycle since 1987. The company serves more than 600,000 residents and supplies approximately 42 hm³ of drinking water. The system operates at a flow rate of up to 2 m³/s, ensuring urban water supply through an extensive pipeline network of around 2,000 km, divided into approximately 240 DMAs (District Metered Areas) and equipped with over 240,000 meters, 170,000 of which are smart devices. -
-
-
Enhancing resilience for London’s Silvertown Tunnel, a major piece of transport infrastructure
Discover how Xylem delivered six pumping stations to prevent flooding in London’s new Silvertown Tunnel, ensuring safe, reliable transport for 25,000 vehicles daily.
-
EnviroMix AquaBlend delivers high-quality drinking water in Montana
Learn how the Montana Law Enforcement Academies used EnviroMix AquaBlend™ technology to prevent water stagnation, reduce maintenance, and improve potable water quality in elevated storage tanks. -
EnviroMix BioCycle-D delivers 45% energy savings in Adairsville, GA
Read how Adairsville’s North WWTP reduced aerobic digestion energy use with EnviroMix BioCycle-D by decoupling aeration from mixing and using automated aerobic and anoxic cycles, delivering more than 45% energy savings versus conventional diffused air mixing. -
EnviroMix BioCycle-D delivers AL plant low-maintenance aerobic digestion
Read how the Eastside Wastewater Treatment Plant in Albertville, AL used the EnviroMix BioCycle-D™ process to simplify operations, reduce maintenance, and improve energy efficiency. -
EnviroMix BioCycle-D helps WRF meet phosphorus limits in Detroit Lakes, MN
Read how Detroit Lakes, Minnesota met a 0.066 mg/L phosphorus limit by upgrading aerobic digestion with EnviroMix BioCycle-D, delivering 77% energy savings and over $100,000 in annual power cost savings while keeping phosphorus sequestered in the sludge. -
EnviroMix BioMix enhances BNR and reduces DO in Orlando, FL
See how Orlando’s Water Conserv II WRF improved denitrification by replacing diffused-air mixing with EnviroMix BioMix to lower dissolved oxygen in anoxic basins, reduce long-term O&M costs, and strengthen BNR performance and resiliency after high-flow events. -
EnviroMix BioMix helps HRSD keep Chesapeake Bay clean
Read how HRSD used EnviroMix BioMix™ technology to improve biological nutrient removal, increase operational flexibility, and reduce O&M costs at the VIP Wastewater Treatment Plant. -
EnviroMix BioMix minimizes maintenance for WI cheese maker
Read how Mullins Cheese used EnviroMix BioMix™ technology to reduce maintenance, optimize aeration control, and improve mixing efficiency in its wastewater treatment process. -
EnviroMix BioMix provides O&M savings in Russellville, AR
See how Russellville’s Pollution Control Works reduced operating costs with BioMix compressed gas mixing and achieved 75% energy savings in Phase I and more than 60% in Phase II versus mechanical mixers. -
EnviroMix BioMix reduces energy and maintenance in Broomfield, CO
See how Broomfield’s Wastewater Reclamation Facility improved thickened sludge holding tank mixing with EnviroMix BioMix and reduced energy use by more than 50% versus coarse bubble aeration, saving about $10,000 annually.