-
Xylem’s Flojet Technology Supports Advanced Solution to Replenish First Foods in the Western U.S.
The Confederated Tribes of the Umatilla Indian Reservation (CTUIR) is a sovereign governmental nation made up of three Native American tribes – Cayuse, Umatilla, and Walla Walla.
-
Empowering Data-Driven Pipeline Management
This guide, developed in partnership with AWWA, explores how utilities can adopt data-driven pipeline management strategies and features real-world utility success stories. Learn more about assessing pipelines and leveraging data to prioritize and address risk.
-
The first Hydrovar X installation in the UK – PressBoost LtD
Recognising the urgency of the situation, PressBoost’s engineering team swiftly arranged the installation of the booster set unit to restore the water supply in the building the same day.
-
-
Preventing Rising Main Failures: Leveraging Inspection Data for Proactive Rising Main Management
Most rising mains failures are preventable. And today, inspecting them is easier, more cost-effective, and less disruptive than ever, thanks to the development of advanced inspection technology such as Xylem’s SmartBall.
-
Xylem and FoodJet Partner on World-First Sauce Depositing Machine with Adaptive Capabilities
With a long history in engineering and developing high-tech equipment for the food industry, FoodJet has established itself as the world’s first and leading company in precision depositing machinery, offering bespoke solutions for industrial food producers. In response to the demand for more consumer choice, including the need for food producers to supply smaller and more irregular shaped pizzas, FoodJet developed the MDL pizza sauce depositor...
-
Durability and 24/7 reliability
Tasked with transferring water from settling ponds to a frac pond for project in mid-Western U.S., a specialist water provider to oil and gas drilling companies needed a pump capable of handling a complex operation through a seven-mile-long steel pipeline.
-
Pump replacement project at Gloucester Docks keeps Bristol’s water supply flowing
The four existing column pumps at Gloucester Docks - which are vital for managing water levels in the canal and keeping Bristol’s water supply running - were reaching the end of their working life and needed replacement.
-
Scottish Water deploy SoundPrint® Acoustic Fibre Optic System
Scottish Water partnered with WRc and Xylem to inspect the Blairlinnans water main using SmartBall® acoustic leak detection platform and PipeDiver™ electromagnetic condition assessment technology in combination with detailed engineering analysis.
-
Xylem and HomeBiogas partner to improve sanitation for communities lacking access to basic toilet facilities
HomeBiogas identified the possibility to support the development and transformation of such communities through the use of their patented Bio-Toilet, a compact and portable waste management solution that converts waste into renewable biogas for cooking – all without the need for electricity.
-
Flygt Concertor Eradicates Wastewater Pump Blockages for Yorkshire Water
Yorkshire Water’s Dynamic Maintenance Team identified that they required an easily deployable solution that delivered tangible benefits across the network.
-
Guide to Monitoring Impact of Storm Overflow
The Environment Act 21 became law in November 2021 and sets out ambitious targets for the protection of our rivers, estuaries, and coastal zones. Part 5 Section 82 requires water utilities to continuously monitoring water quality upstream and downstream of all storm overflow and sewage disposal works, which discharge into a water course.
-
Smith-Blair Bell Pack Stops Leaking Sewer Force Main in Miami
The sewer force main was not just leaking into the streets but into the Intercoastal Waterways along the coast of Florida. Smith-Blair engineers developed the solution, sent drawings to the customer, got the drawings approved and then had fabrications team come in specifically to work on the 48 inch bell pack all night.
-
Smith-Blair Dismantling Joint Used In The Panama Canal
The dismantling fitting will allow for easy removal and re-installation of the butterfly valve when valve maintenance is required. These fittings are part of the new Panamanian subway system pipeline relocation project that involves several thousand feet of pipeline.
-
Smith-Blair Flanged Coupling Adapter in Central Florida
For this particular job, Smith-Blair built 36 inch Flanged Coupling Adapters (FCAs). The FCAs are designed to provide an efficient means to remove and reinstall the pumps, valves and other fittings during maintenance procedures.
-
Xylem and Fabricon Group Collaborate on Innovative Sanitation Solution for Dogs
Having noticed a gap in the market, Fabricon Group designed and manufactured an innovative shower unit specifically for dogs that could sit alongside other domestic appliances in a kitchen or utility room setting, making it more accessible. The shower is plumbed using a hot and cold feed for extra comfort, and water is drained from the system via a specialized pump.
-
Building a Sustainable Future: Solving modern building challenges with hydronics
A new white paper from Bell & Gossett explores the value of hydronics in reducing HVAC systems’ negative impact on the environment and advancing sustainability, decarbonization and net zero emissions
-
Xylem’s Flojet Brand and Flow Loop Partner on Innovative and Sustainable Shower Solution
Body care, including showering and bathing, is the biggest water consuming activity within domestic households, accounting for around 40% of daily consumption. In a bid to make showering more water efficient, Danish start-up company Flow Loop designed the ‘LOOP’ – a sustainable yet luxurious recycling shower solution that reduces water consumption by 80%.
-
Application of Index Velocity Method in Complex Flow Conditions
Flow monitoring site and hydraulic conditions that can impact a stable stage-discharge relationship comprises of unstable section control, sediment transport, debris, vegetation, off-channel storage, variable backwater effects and unsteady flow conditions.
-
Installation of online water quality monitoring systems enabled Thames Water to protect a key clean water treatment works from four separate catchment pollution incidents
Online water quality monitoring systems were deployed to protect treatment processes, improve resilience and ensure availability of clean water to the customers supplies.
-
Variable Speed Pressure Boosters and Hydropneumatic Tanks
One of the key advantages of a variable speed system as opposed to the constant speed systems of old is the ability to adjust pump speed and staging in relation to actual demand or changes in incoming city pressure.
-
Diffuser Liquid Cleaning Saves Treatment Plant 50,000 kWh Per Year
In September 2021, the Veszprém wastewater treatment plant engaged Sanitaire to provide diffuser liquid cleaning service, which uses formic acid injected into the main aeration pipe to clean the diffuser membranes while they are operating.
-
Specification Tips to Maximize Heat Transfer
Heat exchangers are widely used in various industries including chemical, oil & gas, power generation, food & beverage, HVAC & refrigeration, pulp & paper to name a few, and are expecting strong growth over the coming years driven in part by a rising focus on environmental impact and improving efficiency standards.
-
Xylem’s smart condition monitoring device helps US-based global metal processing company move one step ahead of pump failures
An inspection of the pump showed that the internals had been severely damaged by overheating. The plant operators arranged for the pump to be repaired off-site at Xylem’s Morton Grove facility before being returned for recommissioning.