It looks like you are coming from United States, but the current site you have selected to visit is Angola. Do you want to change site?

Yes, please! No, keep me on the current site

Finnish shipyard improves dry dock dewatering with smart submersible pumps

The Suomenlinna shipyard in Helsinki, Finland, one of the country’s oldest operational shipyards, modernized its dry dock dewatering with Flygt N3171 submersible pumps to improve efficiency and reliability. Smart submersible pumps with adaptive performance and remote monitoring were introduced to manage seawater, groundwater seepage, and frequent dock emptying while reducing manual work and energy consumption.

fevereiro 23, 2024
Industrial Construction & Dewatering

Built in 1750, the Suomenlinna shipyard is a UNESCO World Heritage site that still has two active dry docks. The shipyard is part of the Suomenlinna Sea Fortress, located on islands off Helsinki’s coast and visited by about one million people per year. When the site’s managers needed a more efficient way to empty the dry docks, they chose Xylem’s Flygt N3171 submersible pumps, with remote monitoring and adaptive performance to save energy.

The fortress and shipyard were built when Finland was still part of Sweden, serving as a base for the Swedish Coastal Fleet. The location of the shipyard and its dry docks was ideal because there was a natural inlet between the main island with the fortress and the smaller islands around it.

Over the years, the shipyard has served many purposes. It was used to manufacture airplanes in the early 1900s, as a submarine base in the 1930s, and as a place to build ships after World War II. Today the fortress and shipyard are one of Finland’s most popular tourist destinations, with more than 400 people working on the islands and 800 people living there.

Docking and renovating traditional sailing ships

The shipyard is now managed by Viaporin Telakka Ry, an association that aims to preserve knowledge and skills related to old sailing ships and their restoration. The association uses the shipyard’s indoor dry dock to house 20 old wooden and iron ships over the winter, and it uses the outdoor dry dock throughout the year for repairs on smaller ships.

“The indoor dry dock is 50x140 meters and can hold about 42,000 cubic meters of seawater,” says Oskari Reipas, Supervisor of Technical Building Management at Suomenlinna. “It is emptied between October and November every year and filled again in the spring. The outdoor dry dock is 21x120 meters, about 15,000 cubic meters, and it is emptied about twenty times a year.”

The challenge of keeping the docks dry

Reipas says that dewatering the docks was a difficult, time-consuming process. Even after the main pump in a pumping station emptied the docks, they would start to fill up again due to groundwater seepage and rainwater.

"To keep the docks dry, we had to use three separate pumps, which were moved according to the situation,” says Reipas. “The largest pump was so heavy that a pulley had to be used to move it. In the winter, we also had to use temporary hoses that were inconvenient. We had to check the situation once every couple of days, because there was no remote monitoring of the pumps.”

Flygt pumps dewater docks and save energy

To solve these challenges, the shipyard decided to look for a new pumping solution. They selected two Flygt N3171 22 kW submersible pumps from Xylem, which were connected to the main pump. Able to pump 140 liters per second, the pumps also included pressure sensors and variable frequency drives.

“We installed the Flygt SmartRun variable frequency drives in the pumps, which allow the pumps to adapt their performance based on water conditions. This means that the pumps always run at the optimal speed, helping the shipyard save energy.”
Janne Joutsensalmi, Sales Manager, Xylem

Xylem’s Janne Joutsensalmi (left) and Suomenlinna's Oskari Reipas inspect a dry dock.

Xylem was also responsible for installing the pumps, which was a smooth process since the shipyard had prepared all the pipelines in advance. 

“We can now remotely monitor the pumps and their data from the shipyard’s control room,” says Reipas. “This makes our busy days so much easier, and the new pumps make dewatering the dry docks much simpler.”

Improving efficiency and saving energy

By modernizing dry dock dewatering with smart submersible pumps, the Suomenlinna shipyard reduced manual work, improved reliability, and lowered energy use while continuing daily operations at a complex, historic site. By supporting smarter operations, Xylem contributes to more prosperous economies built on reliable, cost-effective infrastructure.