Bombas de impulsor de canal Flygt

C-3000

BOMBAS DE IMPULSOR DE CANAL

  • Impulsores anti-obstrução
  • Designs de palhetas simples e múltiplas
  • Designs tradicionais de grande porte
  • Alta eficiência de água limpa
  • Ferro fundido e materiais opcionais para o impulsor

Need help?

Contact an Expert
Pump Models Technology Case Studies & White Papers
Pump Models
There are no results that match your search
Technology

BOMBAS DE IMPULSOR DE CANAL FLYGT

 As bombas C do impulsor de canal Flygt são construídas para manusear capacidades de até 3.000 l/s (48000 gpm) com motores até 775 kW (1050 hp). As versões de base dessas bombas são fabricadas em ferro fundido duradouro e destinam-se a aplicações exigentes, como águas residuais urbanas e efluente industrial. Estão disponíveis versões à prova de explosão. As clássicas bombas C com impulsores de palheta única e múltipla comprovaram a sua qualidade ao longo dos anos. As bombas C mais pequenas vêm equipadas com o impulsor Flygt Nevaclog®, que possui grandes propriedades de passagem de sólidos por passagens livres. As bombas maiores têm impulsores de palhetas múltiplas para máxima eficiência hidráulica e resistência à obstrução.

Case Studies & White Papers

Circular stormwater pump station

FRANCE

Challenge One of the largest airports serving France required a stormwater treatment plant to handle the inflow from a large gravity sewer collecting water from the runways. Solution The pump station...

Read More

Pump station with cleaning function

SWEDEN

Challenge Eighteen Flygt pump stations transport wastewater at a popular recreational and amusement area in central Stockholm. One of the pump stations handles restaurant wastewater containing fats,...

Read More

Expansion of a desalination plant

AUSTRALIA

Challenge One of Australia’s largest cities was running short of fresh water and needed a major expansion of its desalination facility. One hurdle was to transfer the seawater to the plant. A new...

Read More

Sewage and stormwater pump stations

UK

Challenge The revival of one of Britain’s largest commercially unexploited land areas called for multi-phase construction of two large pump stations. One pump station was to provide drainage for a...

Read More

Large capacity circular wet well

USA

Challenge Very deep, large capacity and limited footprint: these are common demands by customers for their pump stations designs. Recently, two such pump stations were needed in the US. Solution The...

Read More

Circular wastewater lift station

USA

Challenge A 54,000-acre service area in a major city in Texas required assistance to handle a projected 50% increase in population and subsequent increase in wastewater processing demands. Solution...

Read More