-
EnviroMix BioMix reduces energy and maintenance in Broomfield, CO
See how Broomfield’s Wastewater Reclamation Facility improved thickened sludge holding tank mixing with EnviroMix BioMix and reduced energy use by more than 50% versus coarse bubble aeration, saving about $10,000 annually. -
EnviroMix BioCycle-D helps WWTP meet stringent limits in Boxelder, CO
See how Boxelder Sanitation District upgraded its Fort Collins-area WWTP to meet stricter nitrogen and phosphorus limits with EnviroMix BioCycle-D optimized aerobic digestion. The decoupled aeration and mixing approach cut projected energy use by 75% versus conventional estimates and is saving more than $175,000 annually. -
EnviroMix BioMix delivers completely mixed anoxic zones in Ventura, CA
See how Ventura’s Water Reclamation Facility solved sludge settling and septic corners in its BNR anoxic zones by replacing ten submersible mixers with EnviroMix BioMix compressed gas mixing. The result was complete mixing with negligible oxygen transfer and estimated energy and maintenance savings of more than $60,000 per year. -
EnviroMix BioMix provides O&M savings in Russellville, AR
See how Russellville’s Pollution Control Works reduced operating costs with BioMix compressed gas mixing and achieved 75% energy savings in Phase I and more than 60% in Phase II versus mechanical mixers. -
EnviroMix BioCycle-D delivers AL plant low-maintenance aerobic digestion
Read how the Eastside Wastewater Treatment Plant in Albertville, AL used the EnviroMix BioCycle-D™ process to simplify operations, reduce maintenance, and improve energy efficiency. -
ESAMUR: piattaforma completa di digitalizzazione per il monitoraggio avanzato del sistema di depurazione delle acque reflue della regione di Murcia
Il progetto REGEN-IA, sviluppato sulla piattaforma Xylem Vue, nasce con l’obiettivo di integrare, organizzare e valorizzare in un unico ambiente le informazioni operative di ESAMUR. -
Realtime monitoring cuts pollution risk at Scottish Water site
When a critical pumping station failed, Scottish Water used Xylem Vue Secure Connect monitoring and real-time data to restore resilience and protect the environment. -
Beating the blockages at Rochfort Manor
How Flygt Concertor eliminated pump blockages, improved reliability, and delivered over 70% energy savings for Irish Water. -
Zero unplanned failures since 2013
Planned Maintenance Agreement delivers budget predictability and zero unplanned failures for Municipality of Scott -
A clear path forward for City of Kamloops’ most critical feeder main
The City of Kamloops used Xylem's PipeDiver to inspect an aging main, gaining defensible data to extend asset life, plan a repair and refine capital priorities. -
Mimizan: reducing inflow and infiltration through centralized data collection and analysis
The Mimizan Federation of Municipalities is implementing the Xylem Vue platform to reduce inflow and infiltration by improving infrastructure monitoring. -
Mission-critical support: Xylem powers sewage reliability aboard the USS Hornet
To help address the USS Hornet’s urgent wastewater system needs, a Xylem Goulds Water Technology 1GD51G4AA model grinder pump was recommended to replace the damaged unit that serves one of the ship’s critical onboard sewage tanks. This support provided the museum with a reliable, high-quality replacement that restored confidence in an essential system while easing the financial burden on the nonprofit organization. -
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
CABB: gestione ottimizzata della rete fognaria
CABB ha implementato Xylem Vue per ottimizzare la propria rete fognaria, con l'obiettivo di ridurre gli straripamenti delle fognature fino al 10% e garantire la conformità alle normative. -
Pumping system with integrated intelligence eliminates chronic clogging and debris buildup in pump station
The city of Sublimity reduced maintenance costs for a problematic wastewater pump station while creating flow capacity for future residential growth. -
EMALCSA: implementation of a digital twin to support decision-making in water supply network operations
The Empresa Municipal de Aguas de La Coruña (EMALCSA) manages the water cycle in the city of A Coruña and seven neighboring municipalities, serving a total population of 400,000. The utility collects, treats and distributes over 36 million cubic meters of drinking water to 138,000 customers each year, via a network of over 560 kilometers, 26 storage tanks and six pumping stations. -
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
ALJARAFESA: Advanced water cycle asset and work order management
Discover how ALJARAFESA modernized water cycle operations with a unified digital platform that connects asset management, maintenance, and leak detection to improve efficiency, responsiveness, and service delivery. -
Orekan (Navarre Regional Government): early warning system to reduce flood risk
The Autonomous Region of Navarre, located in northern Spain, has a surface area of over 10,000 km² and a population of approximately 680,000, concentrated mainly in the Pamplona metropolitan area. It has a highly complex hydrological system, as it is divided between the Ebro River basin, which covers approximately 90% of the region, and the Cantabrian basin, characterized by short, fast-responding basins. -
Secure in-field firmware updates to support more resilient connected products
EU Cyber Resilience Act: Manufacturers must report vulnerabilities from Sept 2026, with full compliance required by Dec 2027 -
Faster draft beer service with Flojet pumps | Bottoms Up System
For GrinOn Industries, creators of the innovative Bottoms Up draft beer dispenser, the goal has always been simple: deliver great beer to people faster, with less waste and zero compromise on quality. -
Xylem Lowara contribuisce alla rinascita del Molino Stucky
Il cuore del sistema di riscaldamento è costituito da un insieme di pompe centrifughe “In-line”, complete di convertitore di frequenza Hydrovar® modelli FCSH4 150-250/150 e FCS4H 125-200/55; queste distribuiscono l’acqua a 8 sottosistemi di riscaldamento specifici per i vari edifici del complesso. Ogni sottosistema è dotato di una serie di circolatori multivelocità che soddisfano in modo indipendente la domanda di ciascun singolo edificio. -
Gruppo CAP: gestione intelligente della rete idrica tramite analisi avanzata dei dati e pianificazione predittiva degli asset
Gruppo CAP ha adottato Xylem Vue con IA per ottimizzare 6.500 km di rete idrica, riducendo le perdite e migliorando la gestione degli asset. -
Real-time decision support helps cut combined sewer overflow volume by 100 million gallons and reduces capital needed for regulatory compliance
Evansville is located on the north bank of the Ohio River in southwest Indiana. The City’s sewer system, parts of which are more than 100 years old, serves a population of 163,000, with combined sewers making up almost 40 percent of the total sewer area.