Documents
-
-
Global Medical Products Manufacturer Relies on Evoqua for Guaranteed Water Quality
A leader in advanced wound care, consumer wellness and medical devices was having problems with bacteria control in their water system. As a global expert in dealing with the complexities of wound management, the customer provides innovative solutions for advanced wound dressings and topical skin care solutions.
-
Goulds Water Technology dealer goes the extra mile to deliver water to homes outside the reach of municipal water
Chris Hock, owner of North Valley Pump Service, Cave Creek, AZ is a professional residential water systems installer. Chris was approached by a local homebuilder inquiring into the possibility of tapping the municipal water supply contained in a storage tank outside the town of Rio Verde.
-
Hometown H2O program gifts East Texas family with clean, running water
Water Well Trust, a nonprofit partner of Xylem and Hometown H2O, is a domestic water program working to bring access to clean and sustainable water to the more than 2 million Americans without it.
-
Hot to cold, from start to finish
Our technology plays a key part in managing water delivery through all elements of the HVAC cycle. The products can be categorised into those best suited to commercial applications and those for domestic and residential use.
-
-
-
Hydrosurveyor Enables Rapid Indian Railways Bridge Surveys
The HydroSurveyor-M9 system from SonTek, a Xylem brand, is an instrument/technology that Indian Railway has employed to rapidly measure bathymetry data along with velocity data.
-
Industrial wastewater treatment with low profile air strippers
Industrial process and wastewater can contain volatile organic compounds (VOCS) that can have a negative effect on the production process or downstream wastewater treatment processes. In these instances, it is often necessary to put treatment equipment in place to remove the VOCs.
-
Innovative cover installed for waste-to-energy purposes
LaForge Bioenvironmental operates a waste-to-energy facility in a northwest farming community of New Brunswick, Canada. The system is located on a 1,000 acre (405 hectare) mixed farming operation, which includes the LaForge Holsteins dairy.
-
Installation of online water quality monitoring systems enabled Thames Water to protect a key clean water treatment works from four separate catchment pollution incidents
Online water quality monitoring systems were deployed to protect treatment processes, improve resilience and ensure availability of clean water to the customers supplies.
-
Intelligent pumping supports United Utilities' CSO programme
Xylem and United Utilities collaborated to transition 330 sites to just three standardized pump types, simplifying maintenance and cutting inventory by 85%. This smart network rollout also slashes reactive service calls by over 90% while lowering energy consumption by up to 40%. -
Ion exchange services remove groundwater contaminants
California Water Service Company had acquired another water company with approximately 100 connections, in Porterville, California, located in a remote agricultural area of the Central Valley. Their annual well testing had shown levels of nitrate at or near the Maximum Contamination Level (MCL) of 45 ppm and perchlorate was found in the groundwater at levels above the Public Health Goal (PHG) of 10 ppb. A treatment system was needed to remove both these contaminants to ensure quality potable water for the local community.
-
-
Kraft Foods achieves excellent nutrient removals
Due to an expansion in potato chip production, the snack food plant required additional wastewater treatment capacity. It needed to be able to meet strict discharge limits for biochemical oxygen demand (BOD), total suspended solids (TSS), ammonia nitrogen (NH3-N), total nitrogen (TN), and total phosphorus (TP) regulations.
-
Landfill leachate treatment system significantly reduces operations cost
The South Central Counties Solid Waste Agency, located in Hopewell, Pennsylvania needed a cost effective, on-site treatment system to treat 12,500 gpd of leachate and allow for future expansion.
-
-
Logan Township, NJ expands water reclamation facility
Situated on the banks of the Delaware River, Logan Township, New Jersey has a long history of caring for its watershed and natural environment. In the early 70s, the town designed what has been described as “the nation’s first ecologically planned industrial complex,” Pureland Industrial Complex.
-
Low-pressure UV system ensures reliable and sustainable service water supply
The Böseler Goldschmaus GmbH & Co. KG site features its own modern wastewater treatment plant (38,500 ECW). To always ensure high water quality, a reliable solution was sought to keep the proportion of microorganisms, viruses, and multi-resistant germs safely below the prescribed limits without the use of chemicals.
-
Meeting expanding water needs at Jefferson Hospital
AHN Jefferson Hospital is an award-winning healthcare facility that provides comprehensive inpatient and outpatient surgical services in western Pennsylvania. The hospital’s state-of-the-art-surgical suite features an advanced robotic system, which is controlled by the surgeon for minimally invasive surgery.
-
Midas® OCM eliminates odors associated with sewer collection system
In 2004, a major west coast city began construction of two new interceptor sewers. The 12 foot diameter intercept lines relieve hydraulic overloading, but also created a number of turbulent areas where nuisance odors adversely affected the local residential community. These odors were primarily H2S at concentration levels of up to 150 ppm, as well as volatile organic contaminants (VOCs).
-
Milton Sewer Authority reduces wastewater strength by 90%
Settled in 1771 and incorporated into a borough in 1817, Milton is home to approximately 7,000 people in Northumberland County, Pennsylvania, USA. The municipally-owned Milton Regional Sewer Authority (MRSA) serves many residential customers, but a large portion of the MRSA’s wastewater treatment plant's influent comes from the manufacturing facilities of ConAgra Foods, the food giant that produces Chef Boyardee, Healthy Choice, Andy Capp, LaChoy, and Gulden’s Mustard products.
-
Mission-critical support: Xylem powers sewage reliability aboard the USS Hornet
To help address the USS Hornet’s urgent wastewater system needs, a Xylem Goulds Water Technology 1GD51G4AA model grinder pump was recommended to replace the damaged unit that serves one of the ship’s critical onboard sewage tanks. This support provided the museum with a reliable, high-quality replacement that restored confidence in an essential system while easing the financial burden on the nonprofit organization. -
Mobile equipment helps mining operation meet metal limits
In order to expand operations and maintain a water balance in South Carolina’s wet climate, Nevada Goldfields’ Barite Hills gold mining operation required a treatment plant to handle its wastewater. At this mining site, the company extracts gold from soil using a high pH cyanide leaching solution. The process generated large volumes of cyanide and metal laden wastewater, which they had been storing on-site.