Documents
-
-
EnviroMix AquaBlend delivers high-quality drinking water in Montana
Learn how the Montana Law Enforcement Academies used EnviroMix AquaBlend™ technology to prevent water stagnation, reduce maintenance, and improve potable water quality in elevated storage tanks. -
EnviroMix BioCycle-D delivers 45% energy savings in Adairsville, GA
Read how Adairsville’s North WWTP reduced aerobic digestion energy use with EnviroMix BioCycle-D by decoupling aeration from mixing and using automated aerobic and anoxic cycles, delivering more than 45% energy savings versus conventional diffused air mixing. -
EnviroMix BioCycle-D delivers AL plant low-maintenance aerobic digestion
Read how the Eastside Wastewater Treatment Plant in Albertville, AL used the EnviroMix BioCycle-D™ process to simplify operations, reduce maintenance, and improve energy efficiency. -
EnviroMix BioCycle-D helps WRF meet phosphorus limits in Detroit Lakes, MN
Read how Detroit Lakes, Minnesota met a 0.066 mg/L phosphorus limit by upgrading aerobic digestion with EnviroMix BioCycle-D, delivering 77% energy savings and over $100,000 in annual power cost savings while keeping phosphorus sequestered in the sludge. -
EnviroMix BioMix enhances BNR and reduces DO in Orlando, FL
See how Orlando’s Water Conserv II WRF improved denitrification by replacing diffused-air mixing with EnviroMix BioMix to lower dissolved oxygen in anoxic basins, reduce long-term O&M costs, and strengthen BNR performance and resiliency after high-flow events. -
EnviroMix BioMix helps HRSD keep Chesapeake Bay clean
Read how HRSD used EnviroMix BioMix™ technology to improve biological nutrient removal, increase operational flexibility, and reduce O&M costs at the VIP Wastewater Treatment Plant. -
EnviroMix BioMix minimizes maintenance for WI cheese maker
Read how Mullins Cheese used EnviroMix BioMix™ technology to reduce maintenance, optimize aeration control, and improve mixing efficiency in its wastewater treatment process. -
EnviroMix BioMix provides O&M savings in Russellville, AR
See how Russellville’s Pollution Control Works reduced operating costs with BioMix compressed gas mixing and achieved 75% energy savings in Phase I and more than 60% in Phase II versus mechanical mixers. -
EnviroMix BioMix reduces energy and maintenance in Broomfield, CO
See how Broomfield’s Wastewater Reclamation Facility improved thickened sludge holding tank mixing with EnviroMix BioMix and reduced energy use by more than 50% versus coarse bubble aeration, saving about $10,000 annually. -
EnviroMix BioMix reduces O&M costs in Henderson, CO
See how SACWSD’s Williams Monaco WWTP reduced O&M demands by replacing submersible mixers with EnviroMix BioMix compressed gas mixing, delivering 50%+ energy savings for anoxic and anaerobic selectors. -
-
-
-
Xylem's SBR System Installed at Bowling Green, Kentucky
Bowling Green Municipal Utilities (BGMU) provides commercial water and wastewater treatment and electrical power services to a population of more than 60,000 in the community of Bowling Green, KY. In 2010, the BGMU wastewater treatment plant was approaching the end of its useful life, just as the utility’s operating permit was up for renewal.
-
-
Faster draft beer service with Flojet pumps | Bottoms Up System
For GrinOn Industries, creators of the innovative Bottoms Up draft beer dispenser, the goal has always been simple: deliver great beer to people faster, with less waste and zero compromise on quality. -
Fighting Fire and Maximizing Efficiency with Water One® Services
A global firefighting equipment manufacturer used a plant-based, environmentally friendly coolant in their machine shop that was mixed with softened city water for a proper ratio. Due to the alloys in the brass, the company was limited to the types of coolant that would best suit their needs. The plant-based coolant provided an increase in tool life, resulting in significant savings, but it also posed several problems for the machines.
-
Fighting Water Loss: Best Practices to Reduce Non-Revenue Water and Operate Sustainably
Learn best practices for leak detection, pressure management, and smart metering to help utilities address Non-Revenue Water and move toward a more sustainable "watertight" future. This guide offers practical solutions and valuable insights to create a more efficient and equitable water infrastructure.
-
Flygt Concertor eradicates wastewater pump blockages for Yorkshire Water
Yorkshire Water’s Dynamic Maintenance Team identified that they required an easily deployable solution that delivered tangible benefits across the network.
-
Flygt Concertor wastewater pumping system delivers eight years of high efficiency and clog resilience at Heathrow Airport, while halving station energy consumption.
In November 2015, Heathrow Airport’s water services department installed and trialled Xylem’s new state-of-the-art Flygt Concertor intelligent wastewater pumping system, with the intent to solve chronic clogging issues at one of the airport’s more challenging wastewater pumping stations.
-
Flygt hydro turbines prove to be smart solution for small-scale hydroelectric power project
Even in coal-dominated Kentucky, renewable energy is getting more attention as federal and state tax incentives add up, and the federal government moves closer to capping carbon dioxide emissions and making coal power more expensive.
-
Food Processor Upgrades Boiler Feedwater System to Meet Peak Demand
The protein processor’s existing 75 gpm boiler feed RO system was aging and struggling to meet peak demand for treated feedwater. It also lacked the capacity to support a planned plant expansion. To address this, the processor decided to install a new primary RO system and keep the legacy unit as a backup.
-
German sugar factory controls cooling circuit disinfection
Südzucker produces 5.4 million tons of sugar a year. Situated in Obrigheim, located in the Palatinate region, the Offstein Sugar Factory is one of the largest and oldest of nine sugar factories in Germany. Yearly, 1.4 to 1.8 million tons of sugar beets are processed. During the harvesting campaign (September to December), this is about 16,000 tons of beets daily - around the clock. Syrup and sugar are produced from the beets.