It looks like you are coming from United States, but the current site you have selected to visit is Equatorial Guinea. Do you want to change site?

Yes, please! No, keep me on the current site

Managing air in hydronic systems - an introduction

Join Xylem’s Bell & Gossett to discuss the importance of managing air in hydronic systems.

Managing air in hydronic systems - an introduction

Join Xylem’s Bell & Gossett to discuss the importance of managing air in hydronic systems. 

In this session, Xylem will discuss the following learning objectives for attendees:

  • Highlight the strategies used to control air and use it to for the stability of any closed loop system.
  • Introduce some common mechanisms that allow for air elimination.
  • Discuss the importance of expansion tanks and other pressurization devices in maintaining appropriate system pressure.

Note: All registrants will receive a recording via email after the webinar.

Managing Air in Hydronic Systems - An Introduction

Now available on demand!

Watch Now

CEU and accreditation details

The webinar is scheduled for 1 hour, with the instructional portion approximately 45-50 minutes in duration, and the remaining time for attendee questions answered by your presenter. As an attendee, we recognize you may have the need to acquire documentation verifying your participation. In your registration application, we ask if you require a Certificate of Attendance or Certificate of IACET Approved Continuing Education Units.

The Bell & Gossett Little Red Schoolhouse has been accredited through the International Association for Continuing Education and Training (IACET). As such, we are authorized to provide Continuing Education Units (CEU’s) in accordance with the ANSI/IACET standards.

Attendees will have the option to receive either a Certificate of Attendance, or Certificate for 1 hour of IACET approved Continuing Education Units (0.1 CEU) at the conclusion of the webinar.

As a participant in our live, or recorded, webinar training session, who is seeking a Certificate of Attendance, you have an obligation to fulfill the following requirements:

  • Registered for course on your behalf only
  • Must remain in attendance for the scheduled duration of time
  • At the conclusion of the training session, complete a 5 question seminar evaluation

As a participant in our live, or recorded, webinar training session, who is seeking a Certificate of Completion with applicable number of IACET Approved CEU’s, in addition to the requirements noted above, you must:

  • Take a six (6) question quiz, and achieve a score of 65% or better. (4 or more correct answers)
  • You will be given five (5) attempts to successfully pass the quiz. Notification of score, including listing of correct and incorrect answers, will be sent to you via e-mail within 30 minutes of each completed quiz submission.
  • If a passing score is not obtained after 5 attempts, you will be required to watch the recorded version of the training session in its’ entirety, and then five (5) additional attempts to pass the quiz will be made available.
  • Your certificate will be issued upon completion.

Upon completion of the webinar, please allow for up to 24 hours to receive the email with a link to begin the evaluation and certification process.