-
SIBA: a hypervision platform to anticipate flood risks across Arcachon Bay
SIBA is deploying Xylem Vue to bring its data and hydraulic models together in a single environment, with one clear objective: to improve its ability to anticipate natural hazards and provide predictive insights into flood risk across Arcachon Bay in France. -
Osby Municipality cuts emergency wastewater pump callouts with Flygt Concertor
Osby was dealing with frequent pump clogs and after-hours callouts. After installing Flygt Concertor, emergency interventions dropped sharply and the team gained more time for planned maintenance. -
Beverage producer scales production through water reuse and recovery
Learn how a California beverage producer supported a 400% production expansion by upgrading its reverse osmosis system, increasing water recovery from 65% to 87%, and reducing wastewater discharge. -
Temporary pumping ensures continuous service during asset replacement
After an unexpected wastewater pump failure, Xylem rapidly installed a temporary NC200 Electric unit integrated with the site’s existing pipework, power and controls to maintain uninterrupted operation during the replacement lead time. Variable speed control and 24/7 Secure Connect monitoring ensured efficient, reliable performance throughout the extended hire period, even when a second pump failed. -
Powering one of India's largest semiconductor manufacturers with Ionpure® CEDI
Discover how Xylem's Ionpure® CEDI solution helped one of India's largest semiconductor manufacturers achieve reliable ultrapure water production with a compact, chemical-free system and more than 45% reduced footprint. -
Loches Sud Touraine cuts pump station maintenance by 90% with Flygt Concertor
Serving 50,000+ residents across a network of 220 pumping stations, Loches Sud Touraine piloted Flygt Concertor at two priority sites—turning frequent clog-related callouts into a scalable upgrade path for the wider region. -
Atlantic Beef Products unlocks growth with wastewater treatment upgrade
Atlantic Beef Products needed more wastewater treatment capacity to support plant growth and the addition of tripe processing. Working with Environmental Industrial Services Inc. (EISI), Xylem modernized the facility's treatment system by implementing membrane bioreactor (MBR) technology and automating key processes while maximizing existing infrastructure. -
Bringing modern efficiency to a historic leisure landmark
Working closely with FT Leisure, Xylem supplied Lowara pumps with integrated Hydrovar X drives, delivering a compact, energy-efficient solution that reduced control panel requirements through pump-mounted variable speed control. The approach simplified system design and installation while helping keep the refurbishment project on schedule. -
Meeting stringent copper discharge requirements in cooling tower blowdown
Xylem delivered a compact, portable ion exchange system with SCU metals-removal media and pre-treatment to reduce copper in cooling tower blowdown to the 0.03 ppm discharge limit. Ongoing AQUA pro service support helps keep the system operating reliably with minimal downtime. -
Centro de datos de alto rendimiento que reduce el riesgo de refrigeración con una estrategia de tratamiento de agua por fases
Líder mundial en infraestructuras de centros de datos, diseñado para construir un campus informático a gran escala y de alto rendimiento en el sur de EE. UU. Construido para ofrecer un rendimiento extremo, con topologías eléctricas redundantes, SAI completo y batería de reserva y densidades de bastidor muy altas, las instalaciones necesitaban un sistema de filtrado de agua igualmente resistente para soportar el agua refrigerada primaria y la refrigeración adiabática del enfriador. Con una capacidad de potencia de varios gigavatios, todos los sistemas tenían que diseñarse en torno a un único imperativo: el funcionamiento continuo. -
Sin margen para tiempo de inactividad: Tratamiento de agua de refrigeración redundante para un centro de datos de hiperescala
Un importante operador de hiperescala lanzó un nuevo campus de centros de datos en Virginia con un claro mandato: diseñar infraestructuras de refrigeración para evitar tiempos de inactividad. Con requisitos de alta disponibilidad y estrictas restricciones de descarga, el equipo del proyecto necesitaba un socio de tratamiento de agua que pudiera ofrecer rápidamente, adaptarse a los cambios de diseño a mitad de la corriente y crear redundancia en cada componente crítico. -
Rennes Métropole cuts wastewater overflows into the Vilaine River with smart pumping
Rennes Métropole modernized the Constant Véron pumping station upstream of the Beaurade wastewater treatment plant, replacing aging equipment with intelligent Flygt Concertor® pumps. The upgrade increased wet-weather handling and helped prevent overflows to the Vilaine River—delivering higher throughput with stable energy use in the existing footprint. -
Advanced filtration technology transforms Gronau (Leine) outdoor pool in Germany
At the Gronau (Leine) outdoor pool, the forward-thinking and space-saving Defender precoat filter is replacing the old sand filtration systems. -
Friesland Campina simplifies wastewater management with a long-term service agreement
Xylem automates, upgrades and expands key processes and improves effluent quality through a design-build-own-operate agreement -
Comunidad de Regantes de Llíria: digitalización integral del regadío para la mejora de la eficiencia y resiliencia operativa
La implantación de una solución integrada, basada en la plataforma Xylem Vue, ha permitido a la Comunidad evolucionar hacia una gestión digital, centralizada y en tiempo real del sistema. -
Servicios de Agua Drenaje de Monterrey: Reducing non-revenue water and controlling pressure
Regulate and monitor pressures, supervise flow rates, consumption, and non-revenue water (NRW) in different sectors, and bring together system information from various sources including the SADM’s SCADA.
-
Triple A Barranquilla: Controlling water loss and integrating water system management
Improve hydraulic efficiency of the water distribution system for the City of Barranquilla, Colombia and its 14 surrounding municipalities and reduce non-revenue water losses, which were around 50%.
-
CCACVI: Acquisition, implementation, hosting and maintenance of a hypervision solution for water and sanitation systems
The French Community of Communes Albères Côte Vermeille Illibéris (CCACVI) is promoting a hypervision project to streamline its water cycle, based on the Xylem Vue platform. -
Intelligent pumping supports United Utilities' CSO programme
Xylem and United Utilities collaborated to transition 330 sites to just three standardized pump types, simplifying maintenance and cutting inventory by 85%. This smart network rollout also slashes reactive service calls by over 90% while lowering energy consumption by up to 40%. -
Sustainable ultrapure water for solar manufacturing
A leading solar manufacturing facility in India required a reliable, high-capacity ultrapure water solution to support large-scale production while reducing environmental impact and operational complexity. -
La solución de Xylem resuelve las infracciones de permisos de descarga de aguas pluviales
Una refinería del sur de California resolvió las infracciones de los permisos de descarga de aguas pluviales en cinco días utilizando el sistema de tratamiento basado en buques de Xylem con organolay, carbono e intercambio de iones para eliminar hidrocarburos y metales a niveles de ppb.
-
Gobierno del Principado de Asturias: implementación de un DataHub del ciclo integral del agua a escala regional
La solución se articula como un DataHub regional basado en la plataforma Xylem Vue, orientado a integrar y visualizar información del ciclo del agua a escala autonómica. -
CGUCJT: sistema de ayuda a la decisión en el sistema de riego del Canal Júcar-Turia
La plataforma Agrotwin, de Xylem Vue, ha permitido a la CGUCJT avanzar hacia una gestión digital, centralizada y en tiempo real del sistema de riego en alta del Canal Júcar-Turia. -
Ciudad de Mánchester: Captura y reutilización eficiente de aguas pluviales a través de datos y análisis
El Manchester City FC utiliza tecnología inteligente y reutilización de aguas pluviales para reducir el uso de agua potable en su campus Etihad. Con la ayuda de la plataforma basada en datos de Xylem, el club tiene como objetivo optimizar la irrigación y lograr una reutilización completa de las aguas pluviales para 2026.