-
Article
EnviroMix’s operational excellence award presented to Loveland, CO
In January 2023, EnviroMix recognized the Loveland, Colorado WRF with its Operational Excellence Award for strong operations and BioMix performance. -
Article
EnviroMix’s operational excellence award presented to Orlando, FL
In April 2022, EnviroMix recognized Orlando’s Water Conserv II WRF with its inaugural Operational Excellence Award for strong operations and BioMix performance. -
Article
EnviroMix’s operational excellence award presented to Ventura, CA
In February 2024, EnviroMix recognized the Ventura, California WRF with its Operational Excellence Award for strong operations and BioMix performance. -
Article
EnviroMix’s operational excellence award presented to Warren, MI
In November 2022, EnviroMix recognized the City of Warren, Michigan WRF staff with its Operational Excellence Award for strong operations and BioMix performance. -
Article
EnviroMix BioMix-DC system earns WEF innovative technology award
EnviroMix’s BioMix-DC Enhanced Anaerobic Mixing System was selected as a 2022 WEF Innovative Technology Award winner. -
Article
The revised Urban Wastewater Treatment Directive: Why it’s time to act
Learn how wastewater treatment plants can prepare for the revised UWWTD, improve performance and unlock long-term operational benefits with Xylem. -
Article
Stormwater treatment in a changing regulatory landscape
Stormwater treatment under the revised UWWTD is raising the bar, and CoMag™ ballasted clarification helps utilities increase peak-flow capacity and compliance without expanding plant footprint. -
Article
HVAC energy efficiency: reducing consumption in existing systems with advanced control technologies
Strategies and technologies for modernising heating and cooling systems in residential and commercial buildings. -
Article
How total water management supports dairy processing growth
Learn how total water management helps dairy processors expand production, optimize wastewater treatment, reduce costs, and prepare for changing regulations. -
Article
Rising electricity demand makes water reliability critical for nuclear power
Learn how water treatment, ion exchange resin, and expert technical support help nuclear power plants improve reliability, maximize uptime, and meet growing electricity demand. -
Article
Más allá de la bomba: cómo los circuladores inteligentes están cambiando el rendimiento HVAC
A los proyectistas e instaladores se les pide que suministren sistemas de calefacción y refrigeración que sean eficientes, fiables, fáciles de poner en marcha y cómodos para el usuario final. Además, deben hacerlo en un mercado marcado por altos precios de la energía, regulaciones más estrictas y diseños de sistemas cada vez más complejos. -
-
Article
Three ways hydronic systems benefit data centers
From lower energy consumption to maximum uptime, modern hydronics deliver substantial advantages -
Article
5 errores a la hora de elegir una bomba de pozo
Los problemas más comunes en las instalaciones de edificios y cómo evitarlos desde la fase de diseño -
Article
La regulación de las aguas subterráneas se endurece: qué implica la nueva directiva de la UE para los operadores de sondeos – y por qué el control del bombeo marca la diferencia
Con la adopción de la Directiva (UE) 2026/805, la Unión Europea ha reforzado de forma sustancial su marco normativo para la protección de la calidad del agua, sometiendo las aguas subterráneas a un nivel de escrutinio sin precedentes. -
Article
The cost you’re not measuring. How best-in-class efficiency minimises total cost of ownership
When pumping systems are not optimised (oversized duty points, fixed-speed operation, poor hydraulic matching to the actual load profile) every hour of operation is an hour of unnecessary electricity spend. -
Article
Basta de perseguir averías: el mantenimiento programado marca la diferencia
Un enfoque estructurado del mantenimiento permite reducir costes ocultos, prevenir paradas de planta y mejorar la continuidad operativa a largo plazo. -
Article
Three ways liquid cooling presents an opportunity for water use efficiency
ebook explores how liquid cooling can help data centers meet growing AI-driven demands while improving water and energy efficiency through a a system-level approach. -
Article
Powering the HVAC transition: how xylem is enabling the next generation of low-carbon buildings
As energy performance requirements tighten, the need for ultra-efficient pumping solutions is growing fast. Xylem’s ecocirc S, M and L circulators meet this challenge head-on. -
Article
Future-proofing data centres starts when minimum compliance stops
Data centres are under growing technical, regulatory and public pressure. Energy, water and carbon aren’t side issues to manage after commissioning. -
Article
Customer-driven innovation in pharmaceutical water generation
Discover how Xylem's MemGEN™ water generation solution addresses the core challenges of pharmaceutical water systems—lead times, cost control, compliance, and serviceability—through customer-driven design. -
Article
Resiliencia Hidráulica Urbana: por qué el drenaje se ha convertido en una infraestructura crítica
Descubre por qué el drenaje urbano se ha convertido en una infraestructura crítica y qué soluciones técnicas adoptar frente a eventos climáticos extremos. -
Article
Reutilización del agua: REUTILIZAR CERVEZA 2026
Desde las aguas residuales hasta un sorbo sostenible: pioneros en la reutilización del agua. Más información sobre ReUSE BREW, nuestra cerveza hecha de aguas residuales. Leer ahora → -
Article
Más vida útil, menos averías: el valor de hydrovar® X para sistemas OEM
de Michael Somma, Factory Application Engineer, OEM