The future of grid management: how DERMS and the StratusĀ® Evolve Intelligent Grid Platform are revolutionizing energy distribution

Metering Utility Infrastructure

The traditional model of energy distribution is undergoing a drastic shift from centralized generation to a decentralized ecosystem where customers are also producers, and renewable energy sources play a critical yet complex role. This transformation challenges traditional grid operations, which were designed for one-way energy flow, and demands innovative solutions to manage the volatility introduced by distributed energy resources (DERs) like solar, wind, and battery storage. 

To address these challenges, utility leaders must adopt proactive, real-time management strategies. Distributed energy resource management systems (DERMS) and advanced solutions like the Stratus® Evolve intelligent grid platform provide the essential tools for excellence in this new landscape. These technologies form the backbone of a resilient, future-proof grid, enabling utilities to embrace decarbonization and energy independence while maintaining stability and reliability. 

Driving grid resilience through DERMS 

Grid modernization is more than just an industry buzzword; it is an operational necessity. As penetration of behind-the-meter (BTM) and front-of-the-meter (FTM) assets increases, utilities face new challenges in load balancing and voltage regulation. Without visibility and control, these distributed assets can destabilize local feeders, leading to outages and serious safety hazards for line workers.  

A robust DERMS acts as the central nervous system, the brain, of the modern grid. It provides the software solutions and technology required to monitor, manage, and optimize versatile energy resources in real-time. By aggregating these fragmented assets, utilities can transform potential liabilities into valuable grid services. 

However, software alone cannot solve the physical challenges of the grid edge. Effective integrations of DERMS calls for accurate, high-speed data to function effectively. It requires hardware that does more than measure consumption—it needs intelligent endpoints capable of processing data where the action is happening. 

Redefining the grid edge with the Evolve Intelligent Grid Platform 

To bridge the gap between central software control and physical grid assets, Sensus has introduced the Evolve intelligent grid platform. This end-to-end solution represents a departure from traditional metering. It is not merely a device for reads and billing; it is a powerful innovation designed to deliver the granular visibility that is required for strategic decision-making. 

The Evolve platform empowers you to innovate with confidence, offering specific features that directly address the pain points of the utilities we serve. 

Real-time intelligence delivering the right data at the right time 

Speed is the name of the game for grid stability. Relying on data that is 15 minutes or even 24 hours old is insufficient for managing the fluctuations of renewable generation. The Evolve platform embeds intelligence directly into the meter. 

By processing data at the edge, utilities can identify issues—such as voltage sags, swells, or outages—the moment they occur. This capability supports "end-to-end applications," meaning the device doesn't just record an event; it analyzes it. This localized intelligence reduces the latency between detection and action, allowing operators to maintain stability even as load profiles shift rapidly. 

Turning raw data into fast, actionable insights and providing ROI 

Data volume is rarely the problem for modern utilities; data clarity is. We understand that executives need clear insights, not just raw numbers. The Evolve platform integrates seamlessly with Xylem Data Lake (XDL) software to streamline analysis. 

This integration ensures that the vast streams of data collected at the grid edge are instantly consolidated and accessible for utilities to experience immediate ROI. A holistic view of your data with XDL enables:  

  • Proactive transformer loading analysis: Move beyond reactive replacements by identifying overloaded transformers before they fail, extending asset life and improving reliability. 

  • Voltage management: Monitor and analyze voltage sags and swells at the grid edge to optimize power quality and protect sensitive customer equipment. 

  • Streamlined operations with pre-built dashboards: Utilize pre-built dashboards to save valuable time, allowing operational leaders to perform rapid root-cause analysis during disturbances and accurate forecasting for future infrastructure needs. 

For operational leaders, this means ensures you’re equipped with the right data at the right time. Evolve and XDL provide much more than just analytics—they’re the backbone of your intelligent and more resilient utility infrastructure. 

Future-proofing investment through intentional design 

A primary concern for any capital expenditure is obsolescence. In an industry where technology evolves rapidly, committing to hardware with a 15-to-20-year lifespan carries risk. We mitigated this risk with a modular and digital-first approach. 

The Evolve meter features an expansion card slot designed for future upgrades. As new requirements arise, utilities can enhance the device's functionality without a costly rip-and-replace project. This design philosophy protects your investment and ensures that your infrastructure remains adaptable to regulatory changes and technological advancements. DERMS should provide peace of mind and a scalable solution that is truly future-proof.  

Customization with a Linux-based operating system 

No two utilities face identical challenges. An investor-owned utility in a storm-prone coastal city has different priorities than a rural cooperative with vast areas to serve. The Evolve platform acknowledges this diversity by utilizing a Linux-based operating system for customizable solutions. 

This open architecture gives utilities the freedom to deploy tailored applications directly onto the meter. Whether you need specific power quality monitoring apps or custom electric vehicle load disaggregation tools, the platform adapts to your strategic goals. It offers the flexibility to innovate without being locked into a rigid system.  

Unmatched resilience via FlexNet® Communication 

The reliability of a smart grid is only as good as its communication network. During natural disasters—when grid management is most critical—public networks often fail due to congestion or power loss. 

The Evolve platform utilizes FlexNet®, a communication network that operates on licensed spectrum. This ensures a clear, interference-free path for critical data, even during extreme weather events. For added redundancy, the platform also supports complementary communications. This dual approach provides the resilience necessary for disaster recovery and ensures that mission-critical commands reach their destination, guaranteeing service continuity when it matters most. 

Conclusion: partnering for a resilient future 

The decisions made today regarding infrastructure and technology will define utility performance for decades. The move toward a distributed, digitized grid is inevitable, but the success of that transition depends on the tools we employ. 

The Evolve intelligent grid platform is designed to support utilities at every stage of this journey. Whether you are just beginning to integrate smart metering or are looking to optimize a mature DER portfolio, Evolve provides the intelligence, flexibility, and resilience required to succeed. By combining advanced DERMS capabilities with powerful edge computing, we help you build a grid that is not only reliable and efficient but also ready for the future.