The future of energy: AI, data centers, and grid innovation for modern utilities

July 13, 2026
Digital Transformation Metering Utility Infrastructure

As the global energy landscape adjusts to the demands of a rapidly digitizing world, utility professionals are navigating a host of emerging trends and complex challenges. The surge of artificial intelligence (AI) into everyday operations is driving sharp increases in energy consumption, while the explosive growth of data centers is stretching the limits of existing electric grids. Rising expectations for reliability, accelerating electrification, and unfolding regulatory requirements all add to the pressure.

Utilities face difficult questions: How can they deliver stable, high-capacity power to support growing AI workloads? What steps are needed to maintain grid resilience as energy consumption patterns change? And what strategies will safeguard reliability, even as demand surges and the grid becomes more dynamic?

Addressing these challenges calls for strategic shift toward smarter, data-driven operations and future-ready solutions. The Stratus® Evolve intelligent grid platform points to what’s possible: using grid edge insights and advanced analytics to empower utilities with the innovation needed to thrive today and tomorrow.

The AI revolution and next-gen grid management

With the arrival of AI as a pivotal utility tool, the need for real-time, actionable insights has never been greater. Evolve is purpose-built to meet this need, balancing the demand for advanced data today and scalability for tomorrow. This solution empowers utilities to move from reactive to proactive decision-making. With Evolve’s advanced analytics and high-frequency data sampling, utilities gain clear visibility into actual grid conditions as they happen, not just historical trends. This enables automated fault detection, predictive maintenance, and precise load forecasting—unlocking a new level of operational reliability and grid resilience. Building on the foundation of FlexNet® and Evolve, utilities can turn ever-growing streams of grid data into the actionable intelligence needed to avoid outage events, optimize performance, and reliably support the ongoing digital transformation.

This technological advancement addresses the mounting challenges in new energy demands. AI workloads, particularly for machine learning and generative AI, require substantial power. This has accelerated the expansion of data centers, which now rank among the most significant electricity consumers globally.

Data centers and energy infrastructure: building grid stability for the digital era

As energy-intensive data centers rapidly become a staple of the digital economy, utilities are forced to meet rising demand while managing aging infrastructure. They must deliver reliable, high-capacity power, maintain grid stability, and support explosive demand growth simultaneously. The precision management of new generating resources along with the increasing capacity requirements with the influx of data centers, utilities need to minimize the risk of outages. Utilities must enhance their approach to grid management, integrating advanced metering technologies to meet the intensive demands of AI-driven data centers and stay ahead of the curve.

Evolve intelligent grid: powering the edge of what’s next

Evolve stands at the forefront of utility innovation by transforming the electric meter from a passive billing device into an active, intelligent grid sensor. Evolve’s comprehensive grid edge intelligence enables utilities to achieve true real-time system awareness—from substations to every endpoint on the network. Leveraging advanced processing, high-frequency data sampling, and seamless integration with Xylem Data Lake software, Evolve empowers utility teams to mine valuable insights, respond rapidly to changing grid conditions, and optimize performance in a dynamic environment.

With its flexible, Linux-based software architecture, utilities can rapidly develop and deploy custom applications tailored to specific operational challenges, while end-to-end applications provide actionable intelligence for dynamic grid management, faster fault detection, and precise capacity planning. Evolve’s robust communication infrastructure, anchored by the purpose-built FlexNet network, ensures resilient, secure, and scalable connectivity—laying the groundwork for continuous updates, faster integration of new technologies, and utility-specific customization. This future-ready platform empowers utilities to move beyond traditional metering and build adaptable, intelligent, and highly reliable operations.

Strategic innovation and partnership: building the energy future together

The future of energy will be defined by strategic collaboration—where utilities leverage transformative platforms and solutions providers who understand the upcoming trends. Evolve acts as the foundation for innovation, enabling seamless integration, continuous adaptation, and data-driven decision-making across organizations. By providing utilities with a flexible, interoperable, and intelligent grid architecture, Evolve empowers every partner in the energy industry to address evolving challenges, support new technologies, and build a resilient, future-ready grid.

As AI continues to advance and data centers expand, utilities have an unprecedented opportunity to be at the forefront of innovation. By embracing intelligent grid solutions, you can deliver sustainable, efficient, and reliable energy for tomorrow.