Parece que vem de United States, mas o site atual que selecionou visitar é Portugal. Pretende alterar os sites?

Sim. Não. Mantenha-me no site atual.

Rethinking water treatment for micropollutants

Wastewater treatment plays a vital role in protecting public health and the environment. Therefore, the complex challenge of removing micropollutants from water, an emerging problem in recent decades, is high on the agenda for treatment plants worldwide. Here, a process engineer expert at Xylem, discusses how to take control of micropollutant elimination and the role ozone technology is having in project success.   

Micropollutants aren’t a new problem. They are a growing issue though, due to improved detection, the rise of synthetic chemicals and tightening regulation. Micropollutants – including pharmaceutical residues, personal care products, pesticides and industrial chemicals – are typically present in water at extremely low concentrations. Yet, despite their low concentrations, many of these compounds are capable of causing significant impact on aquatic environments, with some compounds persisting in the environment and affecting wildlife even at trace levels.

The challenge of micropollutants

Micropollutants originate from different sources – such as households, hospitals, industrial sites or production facilities - connected to the local sewer system and find their way into wastewater streams. They enter wastewater treatment plants (WWTP) continuously and in complex mixtures, creating significant challenges for treatment operators and regulators alike.

WWTPs act as critical barriers that intercept contaminants before environmental discharge, but they can also become pathways through which trace pollutants enter aquatic ecosystems. Conventional treatment systems, particularly activated sludge processes, were not capable to remove many of the stable and highly soluble compounds now detected in wastewater. This limitation has become increasingly important as environmental monitoring programmes continue to identify micropollutants in rivers, lakes, and coastal waters across the globe. 

For environmental protection and sustainable water management, micropollutant removal has become one of the most important challenges in water treatment today. Governments worldwide are introducing tighter environmental standards and monitoring requirements for emerging contaminants, particularly within Europe and North America. 

One example is the revised EU Urban Wastewater Treatment Directive (UWWTD). Under the updated framework, many larger wastewater treatment plants will be required to introduce advanced treatment processes – accelerating investment in technologies such as ozonation, activated carbon filtration, and membrane systems to improve water quality and reduce risk for aquatic environments.

Advanced treatment 

To meet directive requirements and hit micropollutant removal targets, one of the technologies leading the way is ozone. Ozone is an advanced water and wastewater treatment technology that uses ozone (O₃), a highly reactive form of oxygen, to oxidise and break down contaminants in water. 

Ozone has been used in water treatment for over 100 years, as it’s one of the most powerful oxidising agents available. One of the key advantages of ozone for micropollutant removal is its broad-spectrum treatment capability. Once introduced into water, ozone reacts rapidly with organic compounds, microorganisms, and certain inorganic substances, transforming them into simpler or less harmful forms. Importantly, ozone can reduce colour, odour and taste issues, improve effluent clarity and enhance the overall removal of trace organic contaminants. Because ozone decomposes naturally back into oxygen, it avoids some of the residual by-products associated with traditional chlorine-based disinfection. 

When it comes to eliminating micropollutants, ozone is capable of degrading persistent compounds through direct oxidation or the formation of highly reactive hydroxyl radicals. This dual oxidation mechanism makes ozone highly effective for the treatment of micropollutants that are difficult to remove using conventional biological processes. 

Ozone is typically applied as a tertiary or advanced treatment stage following conventional wastewater treatment, where lower suspended solids and organic loading improve oxidation efficiency.

Today, across Europe more than 80 advanced treatment systems using ozonation are installed or planned in the EU since 2009, including large scale systems and demonstration systems. One example is the Werdhölzli WWTP in Switzerland, which treats the wastewater of Zurich with a design flow of 6,000 l/s (137 MGD). The largest installation in Germany, the Aachen-Soers WWTP, treats up to 3,000 l/s (68 MGD).

Next-generation ozone technology 

It’s imperative that water treatment technology delivers beyond water quality alone to ensure operators can thrive against a challenging operational, economic, and environmental backdrop. Evotide is the perfect example of this. Xylem’s latest ozone system offers next-generation technology for reliable oxidation, along with critical reductions in energy consumption, operating costs, and maintenance time. It is a pre-engineered system for simplified use. Along with its guided user interface, intuitive features, and seamless digital connectivity, Evotide helps reduce downtime and simplify operation – vital for treatment operators. 

Building on decades of research and development, Evotide has unmatched cooling water tolerance, delivering consistent ozone production up to 35°C (95°F). Its Effizon® evo 3G electrodes feature Intelligent Electrode Protection (IEP) to prevent premature electrode failures, for zero downtime and energy-efficient ozone production. Furthermore, the system meets IEEE 519 standards, requiring no external harmonic mitigation equipment. Evotide also meets fire code compliance with IP 65 and NEMA 4 rating, for complete protection against harsh environments. Each of these carefully considered design features helps operators reach water quality targets while maintaining operational efficiency. 

Looking ahead 

There is no escaping that micropollutant removal is rapidly becoming a defining priority for the wastewater treatment sector. Advanced treatment systems sit at the heart of this, and ozone is fast becoming a frontrunner thanks to its powerful treatment capabilities, coupled with vital cost and environmental efficiency benefits. Benefits that plants can’t afford to overlook. It’s time to embrace next-generation water treatment technologies.