It looks like you are coming from United States, but the current site you have selected to visit is Angola. Do you want to change site?

Yes, please! No, keep me on the current site

SIBA: a hypervision platform to anticipate flood risks across Arcachon Bay

SIBA is deploying Xylem Vue to bring its data and hydraulic models together in a single environment, with one clear objective: to improve its ability to anticipate natural hazards and provide predictive insights into flood risk across Arcachon Bay in France. 

Challenge  

Arcachon Bay is exposed to complex hydrological conditions, including rainfall, rising groundwater, watercourses, sea levels and coastal flooding, which can combine to affect both the surrounding area and the stormwater collection system.  

To better understand these interactions, SIBA (Syndicat Intercommunal du Bassin d'Arcachon) has built up an extensive body of data, studies and models over the years. This includes an area-wide hydraulic model that represents drainage networks, watercourses and surface flows, while accounting for rainfall, marine conditions and the hydrogeological context.  

The project aims to make this knowledge readily available to support monitoring and forecasting. Operations teams need rapid access to a clear up-to-date overview of hydraulic conditions across the area and to forecasts of how these conditions are likely to evolve over the coming hours. 

One of the objectives is therefore to provide regularly updated forecasts up to 72 hours in advance, to identify areas that may be affected and anticipate high-risk situations more effectively.  

Solution  

The project is being delivered by the Xylem–Prolog Ingénierie consortium. Prolog Ingénierie will improve and optimize the existing InfoWorks ICM hydraulic models. Once integrated into the Xylem Vue platform, these models will be automatically supplied with available data and used in operations to generate regularly updated forecasts.  

SIBA plans to use Xylem Vue to bring together the data required to monitor rainfall measurements, weather forecasts, groundwater and sea levels, asset data and hydraulic model outputs in the area through a single platform.  

The platform will use this information to forecast how conditions may evolve over the next 72 hours and display areas at risk of flooding directly on a map. Operations teams will have easy access to the information they need to monitor conditions, identify areas requiring particular attention and prepare their response.  

Xylem Vue will also support the monitoring of the different hazards affecting Arcachon Bay, including heavy rainfall, rising groundwater, coastal flooding and erosion. This information will be presented through maps, indicators and alert levels tailored to operational needs.  

Past events can also be replayed and recorded for subsequent analysis to progressively enhance knowledge of the area. Operations teams will be able to review specific events, better understand the processes involved and apply the lessons learned.  

Expected outcomes  

This platform will provide SIBA with a shared view of hydrological conditions across Arcachon Bay, informed by available measurements, forecasts and modelling outputs.  

The solution will enable SIBA to:  

  • anticipate which areas may be at risk of flooding up to 72 hours in advance;  
  • identify priority areas requiring closer monitoring during significant weather events;  
  • use existing hydraulic models in day-to-day operations, with regularly updated data;  
  • learn from past events to improve knowledge of the area and prepare for future events.  

This approach unlocks the value of hydraulic models and data already available to local water authorities by making them readily accessible for monitoring and forecasting. It can also be adapted to other areas facing flood risks that already have an established foundation of data and modelling resources.