It looks like you are coming from United States, but the current site you have selected to visit is Spain. Do you want to change sites?

Yes, please. No. Keep me on the current site.

Nitrogen removal in wastewater treatment

Biological nitrification and denitrification for effective nitrogen removal

Nitrogen removal is a critical part of wastewater treatment. When excess nitrogen is discharged to receiving water, it can contribute to eutrophication, harmful algal blooms, and oxygen depletion that damage aquatic ecosystems. Certain forms of nitrogen, especially ammonia, can also be directly toxic to aquatic life, while nitrate may contribute to downstream water quality and drinking water concerns. Effective nitrogen removal helps treatment plants meet regulatory discharge limits, protect sensitive watersheds, and improve overall effluent quality.

Nitrogen removal is typically achieved through biological processes such as nitrification and denitrification, which convert nitrogen compounds into harmless nitrogen gas to reduce environmental impact.

Biological nitrogen removal processes

Nitrification

Nitrification is the biological process in which aerobic bacteria convert ammonia first into nitrite and then into nitrate. This process takes place in aeration zones with sufficient dissolved oxygen, proper pH, and adequate sludge age. Nitrification is carried out primarily by nitrifying microorganisms growing in activated sludge or biofilm systems.

Denitrification

Denitrification occurs when bacteria convert nitrate into nitrogen gas under anoxic conditions, where dissolved oxygen is absent but nitrate is available. Using organic carbon as an energy source, these microorganisms reduce nitrate stepwise to nitrogen gas, which is released to the atmosphere. Denitrification typically occurs in dedicated anoxic zones.

For optimal denitrification, it is important to provide proper mixing of wastewater flow and return streams, maintain solids in suspension, and prevent measurable oxygen from entering the anoxic zone.

Simultaneous Nitrification and Denitrification (SND)

Simultaneous nitrification and denitrification occurs when ammonia is oxidized to nitrate in aerobic zones while nitrate is reduced to nitrogen gas in low-oxygen microenvironments within the same reactor or floc. Under carefully controlled dissolved oxygen conditions, both nitrifying and denitrifying bacteria can work together to improve nitrogen removal within a single process environment.

Common challenges with nitrogen removal

Nitrogen removal performance can be affected by process stability, energy demand, carbon availability, and permit compliance requirements. Nitrification is sensitive to low dissolved oxygen, cold temperatures, short solids retention time, and toxic or inhibitory compounds, all of which can reduce ammonia removal efficiency. Because nitrifying bacteria grow slowly, recovery after upset conditions can take time. Nitrification also consumes alkalinity and can lower pH, so inadequate buffering may impair performance. In addition, the aeration required for nitrification can make the process energy intensive.

Denitrification depends on maintaining an anoxic environment, providing sufficient nitrate, and ensuring enough readily biodegradable carbon is available. If carbon is limited, nitrate removal may be incomplete and effluent total nitrogen can remain high. In some cases, facilities may need to add an external carbon source, increasing both cost and operational complexity. Poor mixing, dissolved oxygen carryover into anoxic zones, or improper recycle rates can also reduce denitrification efficiency.

For both nitrification and denitrification, effective instrumentation and process control are essential. Variations in influent load, wet weather flow, and seasonal temperature shifts can make optimization difficult. Operators must balance oxygen supply, carbon use, sludge age, and internal recirculation to maintain stable performance. When these factors are not carefully managed, plants may experience ammonia or nitrate breakthrough, lower treatment efficiency, and increased risk of noncompliance.

Proven solutions for nitrogen removal

Xylem works closely with consulting engineers and municipalities to address nitrogen removal challenges. Our comprehensive portfolio and experienced professionals help identify the best options for new treatment plants, retrofits, or upgrades. We offer technologies and services used in biological nitrogen removal, including aeration, mixing, biological treatment, and process monitoring and control.