Parece que vem de United States, mas o site atual que selecionou visitar é Portugal. Pretende alterar os sites?

Sim. Não. Mantenha-me no site atual.

Ative o modo de alto contraste

James River Treatment Plant meets odor control commitments

Evoqua's ArchPro™ low profile cover solution controls odors while providing easy access to tank internals

The James River Treatment Plant is one of nine major treatment plants operated by the Hampton Roads Sanitation District (HRSD), a political subdivision of the Commonwealth of Virginia. Located in Newport News, Virginia, USA, the James River Treatment Plant is committed to protecting the environment and enhancing neighboring communities through a variety of wastewater treatment improvements.

Challenge

The James River Treatment Plant is bordered on one side by the James River, and by houses and a park on the other. Although the James River Treatment Plant had installed odor control systems to capture and treat foul air from parts of the plant, its conventional aeration tanks were producing low-level odors that required additional control. Surrounding residents complained.

The HRSD staff investigated the complaints and worked with neighbors to identify the odor source. An air specialist at the HRSD took samples from various areas at the plant, and even went so far as to bring sample bags to neighbors. Nocardia foam from the aeration tanks was found to be the culprit. Plant management made a commitment to neighbors that the odors would be addressed.

Solution

The plant retained CH2M HILL as its advisor to help solve the odor problem and a decision was made to capture foul air under a cover system so that it could be withdrawn and treated in a carbon system.

A variety of covers were considered. One plan involved covering one portion of the Integrated Fixed Film Activated Sludge (IFAS) tanks with fixed concrete decks that would serve as both covers and mounting surfaces for the scrubbers, and covering the other portion with retractable fabric covers that would provide convenient access to the tank internals. Plant staff participating in the design process noted that they needed to easily access mixers, media, and the spray system within the IFAS tanks.

Plant workers needed the ability to inspect aeration patterns, clean out anoxic sections, and get inside the tanks, when required. These access requirements, along with the possibility of excessive loads that could be imposed on tank walls by concrete lids and scrubbers, led to the decision to design for an alternative scrubber location and cover the tanks entirely with retractable fabric covers instead.

CH2M HILL was aware of retractable fabric covers provided by Evoqua Water Technologies and led an investigation into their merits. The company was selected to provide the cover solution using its retractable structurally supported covers, custom-designed to meet the plant’s specific requirements for access, equipment penetrations, and rainwater management. Evoqua’s ArchPro™ covers consist of retractable, plastic-coated fabric panels tensioned over low-profile, arched aluminum frames.

Later, an ANITA™ Mox treatment system—the only one in the USA right now—was installed to extend the plant’s nutrient removal efforts. The ANITA Mox tank also required a cover for odor control, and because the tank contains mixers, media, and heaters, easy accessibility was again an essential requirement.

"They were able to design and install the cover to fit the conditions of the project. They were always available for questions and input, and did a great job with the installation."
Chris Johnson, Engineer, Town of Ranchester

Results

Evoqua Water Technologies' ArchPro structurally supported covers have helped the James River Treatment Plant continue to be a good neighbor to the surrounding community without hindering plant workers from effectively performing their jobs. “The covers worked out really well,” says Rutherford.

The James River Treatment Plant was mindful to address the odor control issue aesthetically. For example, it was logical to locate the scrubbers near the covers, but it was also important to consider the neighbors’ view. Care was taken in choosing a location for the scrubbers near the tanks, but out of the neighbors’ sight. The covers are low profile and reliably control odors while still providing easy access to tank internals, which was crucial to plant staff.

*ANITA is a trademark of VEOLIA WATER SOLUTIONS & TECHNOLOGIES. All other trademarks are those of their respective owners.