-
Eau d’Azur: France’s first smart water network cuts losses and strengthens drought resilience
The Metropolis of Nice is implementing a hypervision platform, based on Xylem Vue technology, to increase efficiency, sustainability, and resilience by providing a real-time view of the network. -
Thames Water and Xylem set new standard for pump upgrades at scale
A Xylem and Thames Water partnership represents a shift in how water companies can manage inherited infrastructure. -
Scottish Water cuts energy by 60% with Flygt Concertor intelligent pump system
Scottish Water partnered with Xylem to upgrade hundreds of pumping stations with innovative, energy-efficient technology, as part of its commitment to reaching net-zero emissions. -
-
-
Herford utility: cutting CSOs by around 15% using an advanced prevention system
Inconsistent behavior and utilization of control structures was observed for past rainfall events. The municipality decided that an optimized network control system should be implemented to better utilize existing retention volumes, coordinate them effectively and reduce water pollution.
-
Xylem’s Holistic Solution of Mixers and Pumps Supports Efficient Mine Slime Transport – From Sump to Surface Disposal
One customer, operating a hard rock nickel mine in Ontario, needed an efficient and reliable solution to transport its mine slime from an underground sump back to the surface while ensuring continuity in production and minimizing downtime.
-
Flygt Concertor wastewater pumping system delivers eight years of high efficiency and clog resilience at Heathrow Airport, while halving station energy consumption.
In November 2015, Heathrow Airport’s water services department installed and trialled Xylem’s new state-of-the-art Flygt Concertor intelligent wastewater pumping system, with the intent to solve chronic clogging issues at one of the airport’s more challenging wastewater pumping stations.
-
Trial of Flygt Adaptive Mixers Shows Energy and Cost Saving in New Plymouth, New Zealand
Xylem collaborated with the New Plymouth District Council to trial the innovative Flygt Adaptive technology, replacing two existing mixers in the anoxic zone of bioreactors.
-
Xylem bypass system helps facilitate pump station upgrades
Allegheny County Sanitary Authority (ALCOSAN) is a municipal authority that provides wastewater treatment services to 83 communities, including the city of Pittsburgh, reaching a total population of 1.2 million people. -
Welsh Water scales up Xylem’s Flygt Concertor for smarter wastewater management
Dŵr Cymru Welsh Water is scaling up its deployment of Flygt Concertor intelligent pumping systems to improve wastewater network resilience, reduce energy consumption, and support its environmental goals. -
State of the art water treatment technology for a forging works in Saxony, Germany
Various cooling towers are operated in the water treatment plant at the forge. Disinfection is carried out using expensive biocides, which are also environmentally problematic for rivers when discharged directly. The company was therefore looking for new, efficient and cost-effective disinfection technology to solve these issues. -
Nanobubbles enable Meister Cheese to increase cheese & biogas production
Meister Cheese improved wastewater treatment and biogas production using Moleaer's nanobubble technology, saving $10M in CAPAX improvements and doubling cheese output. -
Foul odors eliminated using nanobubble technology at a poultry processor
Miller Poultry cut foul lagoon odors and improved water quality using Moleaer's nanobubble technology, solving odor issues and boosting treatment efficiency. -
Maximizing biogas production through effective mixing technology and active seal protection
Learn more about maximizing biogas production through effective mixing technology and active seal protection. Read our case study with our customer Nesemeier now →
-
Sustainability success for Dairygold: mixers deliver biogas system results that matter
Flygt mixers deliver sustainable success for Dairygold at the heart of the world's largest ADI-BVF® fermenter. Read the case study →
-
Xylem‘s Bell & Gossett and the Academy for Global Citizenship make a powerful investment in education and community
How could more energy, ideas and creativity be created than what is consumed? That is the broader vision behind AGC’s focus on being the most sustainable school of the Midwest, where everything from the classroom to the cafeteria contributes to a climate-friendly output. -
Las bombas Xylem Lowara garantizan un rendimiento de excelencia en el rascacielos más alto del mundo
Xylem Lowara se encuentra en el centro de las tecnologías más recientes en sistemas de transporte de agua y se ha convertido en un proveedor de vanguardia de equipos de bombeo en numerosos proyectos prestigiosos en Oriente Medio.
-
Xylem suministra las bombas para el rascacielos residencial más alto de Londres
Con una altura de 233 m, el edificio es la torre residencial más alta no solo de Londres, sino de toda Europa Occidental. Cuenta con más de 800 apartamentos y servicios como gimnasio y cine privado con capacidad para 24 personas. La construcción se completó en 2020.
-
Low-pressure UV system ensures reliable and sustainable service water supply
The Böseler Goldschmaus GmbH & Co. KG site features its own modern wastewater treatment plant (38,500 ECW). To always ensure high water quality, a reliable solution was sought to keep the proportion of microorganisms, viruses, and multi-resistant germs safely below the prescribed limits without the use of chemicals.
-
New DAF Design Proves Twice As Efficient During Equipment Maintenance
An oil refinery in the US Midwest scheduled repairs to an existing wastewater treatment system. Refinery operations needed a temporary treatment system on site to maintain uptime during the outage. -
Utility transforms operations with Xylem’s Sensus advanced metering solutions
Great Lakes Energy Cooperative (GLE), Michigan’s largest member-owned electric co-op, is in the midst of a multi-year effort to modernize its operations. Serving over 130,000 members, the cooperative launched a project to upgrade its aging power line carrier (PLC) based system to the Sensus FlexNet® communication network in late 2022. -
Hong Kong: development of digital twin pilot for trunk mains water systems in selected areas of New Territories East Region
This project aims to build and calibrate a hydraulic model for trunk mains water systems in selected areas of New Territories East Region and deploy the model through Idrica’s Real-Time What-If-Scenarios solution (now called Xylem Vue).
-
Hong Kong: development of digital twins for freshwater network in selected areas of New Territories East (NTE) Region
Idrica, Xylem´s partner, has delivered its GoAigua solution (now called Xylem Vue) to the Hong Kong Water Supplies Department (WSD) as a pilot project. This deployment aims to develop a digital twin solution customized for the existing freshwater network in selected areas of its NTE Region.