-
Realtime monitoring cuts pollution risk at Scottish Water site
When a critical pumping station failed, Scottish Water used Xylem Vue Secure Connect monitoring and real-time data to restore resilience and protect the environment. -
Beating the blockages at Rochfort Manor
How Flygt Concertor eliminated pump blockages, improved reliability, and delivered over 70% energy savings for Irish Water. -
Zero unplanned failures since 2013
Planned Maintenance Agreement delivers budget predictability and zero unplanned failures for Municipality of Scott -
ESAMUR: plataforma de digitalización integral para la supervisión avanzada de los sistemas de depuración en la Región de Murcia
El proyecto REGEN-IA, articulado sobre la plataforma Xylem Vue, tiene como objetivo integrar, gobernar y explotar la información operativa de ESAMUR en un único entorno. -
A clear path forward for City of Kamloops’ most critical feeder main
The City of Kamloops used Xylem's PipeDiver to inspect an aging main, gaining defensible data to extend asset life, plan a repair and refine capital priorities. -
Mimizan: reducing inflow and infiltration through centralized data collection and analysis
The Mimizan Federation of Municipalities is implementing the Xylem Vue platform to reduce inflow and infiltration by improving infrastructure monitoring. -
Redland city council: Cleveland WWTP operational improvement & data management project with Xylem Vue platform
Redland City Council unified plant operations data with Xylem Vue, boosting compliance monitoring and efficiency at Cleveland WWTP. -
Mission-critical support: Xylem powers sewage reliability aboard the USS Hornet
To help address the USS Hornet’s urgent wastewater system needs, a Xylem Goulds Water Technology 1GD51G4AA model grinder pump was recommended to replace the damaged unit that serves one of the ship’s critical onboard sewage tanks. This support provided the museum with a reliable, high-quality replacement that restored confidence in an essential system while easing the financial burden on the nonprofit organization. -
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
EMALCSA: implementación de un gemelo digital para apoyar la toma de decisiones en la operación de la red de abastecimiento
La Empresa Municipal de Aguas de La Coruña (EMALCSA) gestiona el ciclo integral del agua en la ciudad de A Coruña y en otros siete municipios cercanos, con una población total de 400.000 habitantes. La operadora española capta, potabiliza y distribuye más de 36 millones de metros cúbicos de agua potable a 138.000 clientes cada año, a través de una red de más de 560 kilómetros, 26 depósitos y seis estaciones de bombeo. -
Temporary DAF system supports refinery outage
A temporary wastewater treatment system was deployed during a planned outage to support operations while two existing DAF units underwent repair. -
ALJARAFESA: gestión avanzada de activos y movilidad del ciclo integral del agua
Descubra cómo ALJARAFESA modernizó las operaciones del ciclo del agua mediante una plataforma digital unificada que conecta la gestión de activos, el mantenimiento y la detección de fugas para mejorar la eficiencia, la capacidad de respuesta y la prestación del servicio. -
Orekan (Gobierno de Navarra): Sistema de Alerta Temprana para reducir el riesgo de inundaciones
La Comunidad Foral de Navarra, situada en el norte de España, cuenta con una superficie de más de 10.000 km² y una población aproximada de 680.000 habitantes, concentrada principalmente en el entorno metropolitano de Pamplona. Su territorio presenta una elevada complejidad hidrológica, al estar dividido entre la cuenca del Ebro, que abarca aproximadamente el 90% de la comunidad, y la vertiente cantábrica, caracterizada por cuencas cortas y de respuesta rápida. -
Secure in-field firmware updates to support more resilient connected products
EU Cyber Resilience Act: Manufacturers must report vulnerabilities from Sept 2026, with full compliance required by Dec 2027 -
CABB: optimization of the primary wastewater network
The Bilbao Bizkaia Water Consortium (CABB) is the public utility responsible for managing the main drinking water and wastewater network in the province of Bizkaia, serving over one million residents through a range of water supply pipelines, sewer networks, and wastewater treatment plants across 97 municipalities. -
Xylem Lowara contribuye al renacimiento del Molino Stucky
El corazón del sistema de calefacción incorpora un conjunto de bombas centrífugas “In-line”, equipadas con variadores de frecuencia Hydrovar® modelos FCSH4 150-250/150 y FCS4H 125-200/55; estas distribuyen el agua a 8 subsistemas de calefacción específicos para los distintos edificios del complejo. Cada subsistema incorpora una serie de circuladores multivelocidad que satisfacen de forma independiente la demanda de cada edificio. -
EMASESA: implantación de un gemelo digital del abastecimiento y saneamiento para optimizar la toma de decisiones
Implantación de la plataforma Xylem Vue con el objetivo de optimizar la gestión, anticipar eventos y mejorar la eficiencia, resiliencia y sostenibilidad del ciclo integral del agua en Sevilla. -
Faster draft beer service with Flojet pumps | Bottoms Up System
For GrinOn Industries, creators of the innovative Bottoms Up draft beer dispenser, the goal has always been simple: deliver great beer to people faster, with less waste and zero compromise on quality. -
Gruppo CAP: gestión inteligente de la red de abastecimiento mediante analítica avanzada y planificación predictiva de activos
Gruppo CAP implementó Xylem Vue para optimizar su red de agua de 6.500 km, reduciendo pérdidas y mejorando la gestión de activos. -
Real-time decision support helps cut combined sewer overflow volume by 100 million gallons and reduces capital needed for regulatory compliance
Evansville is located on the north bank of the Ohio River in southwest Indiana. The City’s sewer system, parts of which are more than 100 years old, serves a population of 163,000, with combined sewers making up almost 40 percent of the total sewer area.
-
Global Omnium: Transforming from Conventional to Smart Water
Global Omnium, one of Spain's largest water utilities, has gone through a remarkable digital transformation over the past two decades - upgrading from conventional meters to an advanced smart meter network of over 550,000 fixed network smart meters. This journey provides valuable lessons for any water utility looking to modernize its operations and capitalize on the latest innovations in smart metering and data analytics.
-
EMASA: Incremento de la eficiencia hídrica a partir del análisis inteligente del balance hidráulico
EMASA (Empresa Municipal Aguas de Málaga S.A.) es la empresa pública del Ayuntamiento de Málaga encargada de la gestión integral del ciclo urbano del agua desde 1987. La entidad presta servicio a más de 600.000 habitantes y distribuye aproximadamente 42 hm³ de agua potable. El sistema opera con un caudal de hasta 2 m3/s por segundo, asegurando el abastecimiento urbano a través de una extensa red que alcanza casi 2.000 km de tuberías, está sectorizada en alrededor de 240 DMA y cuenta con más de 240.000 contadores, de los que 170.000 son smart meters. -
City of Mesa pinpoints critical leak, avoiding costly delays
Discover how the City of Mesa, Arizona, used Xylem's SmartBall® technology to pinpoint a hard-to-find pipeline leak, safeguarding infrastructure and avoiding costly delays to a transportation project. -
Publiacqua SpA: Integrating the drinking water management system
Centralize water cycle management for Publiacqua SpA, the utility in charge of providing the drinking water service in Medio Valdarno, in Tuscany, which has four provinces: Florence, Prato, Pistoia and Arezzo.