Documents
-
Flygt hydro turbines prove to be smart solution for small-scale hydroelectric power project
Even in coal-dominated Kentucky, renewable energy is getting more attention as federal and state tax incentives add up, and the federal government moves closer to capping carbon dioxide emissions and making coal power more expensive.
-
-
-
-
Food Processor Upgrades Boiler Feedwater System to Meet Peak Demand
The protein processor’s existing 75 gpm boiler feed RO system was aging and struggling to meet peak demand for treated feedwater. It also lacked the capacity to support a planned plant expansion. To address this, the processor decided to install a new primary RO system and keep the legacy unit as a backup.
-
German sugar factory controls cooling circuit disinfection
Südzucker produces 5.4 million tons of sugar a year. Situated in Obrigheim, located in the Palatinate region, the Offstein Sugar Factory is one of the largest and oldest of nine sugar factories in Germany. Yearly, 1.4 to 1.8 million tons of sugar beets are processed. During the harvesting campaign (September to December), this is about 16,000 tons of beets daily - around the clock. Syrup and sugar are produced from the beets.
-
-
Global Medical Products Manufacturer Relies on Evoqua for Guaranteed Water Quality
A leader in advanced wound care, consumer wellness and medical devices was having problems with bacteria control in their water system. As a global expert in dealing with the complexities of wound management, the customer provides innovative solutions for advanced wound dressings and topical skin care solutions.
-
-
Goulds Water Technology dealer goes the extra mile to deliver water to homes outside the reach of municipal water
Chris Hock, owner of North Valley Pump Service, Cave Creek, AZ is a professional residential water systems installer. Chris was approached by a local homebuilder inquiring into the possibility of tapping the municipal water supply contained in a storage tank outside the town of Rio Verde.
-
Hometown H2O program gifts East Texas family with clean, running water
Water Well Trust, a nonprofit partner of Xylem and Hometown H2O, is a domestic water program working to bring access to clean and sustainable water to the more than 2 million Americans without it.
-
-
Hot to cold, from start to finish
Our technology plays a key part in managing water delivery through all elements of the HVAC cycle. The products can be categorised into those best suited to commercial applications and those for domestic and residential use.
-
-
-
Hydrosurveyor Enables Rapid Indian Railways Bridge Surveys
The HydroSurveyor-M9 system from SonTek, a Xylem brand, is an instrument/technology that Indian Railway has employed to rapidly measure bathymetry data along with velocity data.
-
Improving aerobic sludge digestion efficiency
The aerobic sludge digester cells at the Langley Wastewater Treatment Plant required major overhaul. This was due to limited capacity, sludge overspray from surface aerators and icing conditions that resulted in shutdown. To tackle these challenges, Xylem recommended easy-to-install Flygt jet aerators to boost process efficiency and meet regulatory requirements.
-
-
Industrial wastewater treatment with low profile air strippers
Industrial process and wastewater can contain volatile organic compounds (VOCS) that can have a negative effect on the production process or downstream wastewater treatment processes. In these instances, it is often necessary to put treatment equipment in place to remove the VOCs.
-
Innovative cover installed for waste-to-energy purposes
LaForge Bioenvironmental operates a waste-to-energy facility in a northwest farming community of New Brunswick, Canada. The system is located on a 1,000 acre (405 hectare) mixed farming operation, which includes the LaForge Holsteins dairy.
-
Installation of online water quality monitoring systems enabled Thames Water to protect a key clean water treatment works from four separate catchment pollution incidents
Online water quality monitoring systems were deployed to protect treatment processes, improve resilience and ensure availability of clean water to the customers supplies.
-
Intelligent pumping supports United Utilities' CSO programme
Xylem and United Utilities collaborated to transition 330 sites to just three standardized pump types, simplifying maintenance and cutting inventory by 85%. This smart network rollout also slashes reactive service calls by over 90% while lowering energy consumption by up to 40%. -
Ion exchange services remove groundwater contaminants
California Water Service Company had acquired another water company with approximately 100 connections, in Porterville, California, located in a remote agricultural area of the Central Valley. Their annual well testing had shown levels of nitrate at or near the Maximum Contamination Level (MCL) of 45 ppm and perchlorate was found in the groundwater at levels above the Public Health Goal (PHG) of 10 ppb. A treatment system was needed to remove both these contaminants to ensure quality potable water for the local community.
-
It’s elementary – Xylem goes to the ‘head’ of the class
The best solution for an elementary school in New York was to install two Goulds Water Technology Hydrovar® variable speed frequency drives (VFD) mounted on the existing 5HP SSV Pumps. Selecting this system would provide the constant pressure needed, enhance efficiency, reduce operation and maintenance costs and decrease space requirements.