It looks like you are coming from United States, but the current site you have selected to visit is Tajikistan. Do you want to change site?

Yes, please! No, keep me on the current site

Case Studies

Case Studies

  • Cover System Helps Vallejo Sanitation District Streamline Plant Operations

    The Vallejo Sanitation and Flood Control District is an independent special district created by the State of California to collect and treat wastewater and protect the Vallejo community from flooding. Since 1952, the district has protected public health and the San Francisco Bay Area by treating wastewater generated by the more than 115,000 residents of Vallejo and surrounding area.
  • Covers help keep Kamloops beautiful

    The City of Kamloops is located in the interior of British Columbia, Canada’s westernmost province. Situated along the scenic Thompson River, the city’s wastewater treatment facility currently serves a population of over 80,000 people and treats a daily flow of 40,000 m³ (10 mgd), a number which would soon increase to 60,000 m³ (16 mgd).
  • Disc Filtration Solution Helps WWTP Meet Future Clean Water Needs

    About an hour south of Atlanta, the city of Barnesville, Georgia is a town of shady, tree-lined streets, a fondness for celebrating its history, and a sharp eye on the future. In 2013, as its 30-year-old wastewater treatment plant was reaching the end of its useful life, Barnesville found itself planning for a future of growth, progress, and a new, state-mandated <0.6 mg/L total phosphorus (TP) wastewater discharge limit.
  • Everybody wins at Ho-Chunk Casino in Wisconsin

    At the Ho-Chunk Casino owned and operated by the Ho-Chunk Indian Tribe, thousands of people try their luck. However, at the wastewater treatment facility, customers, suppliers, and engineers win.
  • Xylem selected as a supplier for wastewater treatment pilot facility

    The City of Los Angeles has selected Xylem through its sales partner MiscoWATER, to manufacture and install a wastewater treatment system at the Hyperion Water Reclamation Plant. The new treatment system will be installed as part of a pilot facility to evaluate three membrane bioreactor (MBR) systems.
  • Xylem selected to supply odour control system for Metro Vancouver

    The South Surrey Interceptor is an extensive piping system that collects and conveys approximately 500 million litres of wastewater daily from municipalities in the eastern area of Metro Vancouver to the Annacis Island Wastewater Treatment Plant located in the City of Delta, British Columbia.
  • Xylem's ArchPro™ odor control covers reduce predicted odor impact

    The Cronulla Wastewater Treatment Plant (WWTP) is one of 30 wastewater treatment and water recycling plants in greater Sydney, the Blue Mountains, and the Illawarra. It is owned and operated by Sydney Water, Australia’s largest water utility. The plant is located on the southern end of the Kurnell Peninsula (about 18 km [11 miles] from the city center), and treats about 54 million liters (14 million gallons) of wastewater a day.
  • The Orbal® system for biological nutrient removal

    Water is precious to the 8000 residents of this town in central Utah, as it is to so many similar places in the arid Intermountain West. Town history attributes Salem City's 19th-century founding to its location as a suitable spot for damming up a local spring to create a pond, which is still the centerpiece of the town.
  • Florida city chooses turnkey screw pump replacement solution

    The City of Fort Myers Wastewater Treatment Division includes two regional Advanced Wastewater Treatment Facilities with (6) 11 million-gallon-per-day (mgd) carbon steel Internalift Screw Pumps from Xylem. These pumps were close to reaching their typical life expectancy of 20 years and not operating efficiently.
  • H2S odours eliminated with ZABOCS® system

    A town located in the Western Canadian Rockies prides itself on its natural features that includes a river flowing through the middle of town. The area provides residents and visitors with scenic trails, wildlife habitat, drinking water for the community.
  • Huntertown, IN charts new course with Xylem's Orbal® system

    Just north of Fort Wayne, Indiana, the community of Huntertown boasts the second-fastest growth rate in the state, with no sign of slowing down. An easy commute from the city, attractive neighborhoods and good schools have helped skyrocket its population to nearly 7,000 residents in recent years.
  • Hydro-Clear® filter: a good neighbor at Julington Creek

    Julington Creek is a 4,200-acre (1,700 hectare) planned community, featuring woodlands, lakes, a library, a recreational facility, and 18 holes of golf.  Developed under Florida’s CDD (Community Development District) program, the community is located in south suburban Jacksonville, close to the east bank of the St. John’s River.
  • Hydro-Clear® sand filter rehabilitation

    The Village of Libertyville, Ill., installed a Hydro-Clear® sand filter system from Evoqua Water Technologies in 1977. Since that time, the Village has benefited from the system, making only minor repairs throughout the years.
  • Innovative cover installed for waste-to-energy purposes

    LaForge Bioenvironmental operates a waste-to-energy facility in a northwest farming community of New Brunswick, Canada. The system is located on a 1,000 acre (405 hectare) mixed farming operation, which includes the LaForge Holsteins dairy.
  • James River Treatment Plant meets odor control commitments

    The James River Treatment Plant is one of nine major treatment plants operated by the Hampton Roads Sanitation District (HRSD), a political subdivision of the Commonwealth of Virginia. Located in Newport News, Virginia, USA, the James River Treatment Plant is committed to protecting the environment and enhancing neighboring communities through a variety of wastewater treatment improvements.
  • Liner helps facility return to its regular operations

    The Remington Water Pollution Control Facility needed a liner replacement for one of its basins because the existing liner was old and damaged. The facility had made arrangements for a liner replacement, but the contractor unexpectedly backed out of the agreement to install the liner before the end of the year.
  • Logan Township, NJ expands water reclamation facility

    Situated on the banks of the Delaware River, Logan Township, New Jersey has a long history of caring for its watershed and natural environment. In the early 70s, the town designed what has been described as “the nation’s first ecologically planned industrial complex,” Pureland Industrial Complex.
  • Marathon wastewater treatment plant meets effluent standards

    Like many cities in the Florida Keys, Marathon, Florida had historically used septic systems to treat wastewater.  The community added secondary treatment several years ago, but the facility was unable to prevent nitrogen and phosphorous contamination of sensitive Gulf of Mexico coastal waters.