It looks like you are coming from United States, but the current site you have selected to visit is Tajikistan. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

CHE enhances flood prevention and management in the Ebro river basin

Xylem Vue is helping the Confederación Hidrográfica del Ebro (CHE) reduce flood damage and implement an EWS for stakeholders managing disaster situations in the basin.  CHE is the water authority that manages, regulates and maintains the Ebro river basin, which covers a surface area of around 85,000 km2 and takes in 347 large rivers in northeastern Spain.  

Challenges of the project

The Ebro river basin provides a substantial amount of Spain’s water resources. Its main river, which is 930 km long, flows through different climate zones in the north-east of the Iberian Peninsula, namely the Atlantic, the Mediterranean and a transition area characterized by a broad range of precipitation and transpiration rates. 

The basin’s unique combination of geomorphological and climatological factors, along with the growing impact of climate change, explain the advent of river, pluvial and flash floods in the area throughout the year. The aim of this project was to reduce flood damage and provide an early warning system (EWS) for civil defense and other stakeholders managing disaster situations in the Ebro river basin.

Solution applied

The deployment of the Early Warning System (EWS) application, which is part of the Xylem Vue platform, provides CHE with early warnings during floods in a variety of scenarios. 

The tool computes, analyzes and provides warnings and recommendations based on large amounts of data, provided by hydrological and meteorological sensors, rainfall radar, and weather forecasting models. The application:

  • Uses cloud computing and big data analytics for real-time, probabilistic hydraulic and hydrological modelling. 
  • Applies geo-statistics and machine-learning techniques to improve data quality and leverages its AI inference engine and heuristics for better management recommendations. 
  • Runs every ten minutes and includes a comprehensive, user-friendly interface for enhanced risk warning and awareness. 

The EWS also generates flood maps for different return periods, recommends actions for dams to minimize risks and damage, and helps to send warnings and alerts to selected mobile telephones and websites.

Benefits and results

Thanks to the implementation of the EWS application, CHE can:

  • Respond to different types of floods (localized heavy rainfall, river floods, with/without snowmelt) and anticipate events days or hours before they occur. 
  • Activate disaster management protocols earlier, taking into account information on potentially affected infrastructures and facilities, filtered by population and cost.
  • Evaluate the performance of management protocols, entities, and communications and software systems, after every event to optimize the planning of future efforts and investments.

The EWS also enables CHE to forecast flows and levels accurately, to better understand the current and forecast hydrological status of the basin, and to reduce damage in dams thanks to advanced management.

The implementation of the EWS application, referred to as ‘VIGILAEbro’ by CHE, is in line with the European Floods Directive (2007/60/EC), which includes the need to develop Flood Risk Management Plans.

  • Specific warnings and alerts for stakeholders
  • Earlier activation of disaster management protocols
  • Advanced dam management to protect communities
  • Post-event flood response evaluation

Idrica has carried out this project where the Xylem Vue platform was implemented. Xylem Vue is the result of the partnership between Xylem, a global leader in water technology and Idrica, an international pioneer in water data management, analytics and smart-water solutions. 

Through this partnership, Xylem and Idrica bring together their technology, innovation, and expertise to solve the world’s most critical drinking water, wastewater and other water-related challenges.