It looks like you are coming from United States, but the current site you have selected to visit is Saudi Arabia. Do you want to change sites?

Yes, please. No. Keep me on the current site.

SonTek Total Care Customer Service

Committed to providing the highest level of support for our customers

Need to report a problem or have a general question about your SonTek system? You've come to the right place!

If you are out in the field and need emergency help, call us at +1-858-546-8327. If it is outside our normal business hours, follow the instructions to be connected to one of our on-call support staff, who will be happy to help. 

Whenever you contact SonTek, please be sure to include the serial number of your system. That will help us get to your customer records faster, and give you the timely response you need.

Repair Status Update

If you need a status report on a repair or calibration you recently sent in, this is the place to start. Click through to get the latest information on where your instrument stands in the queue and when you can expect the repair process to be completed.

Repair Status

 

FAQs & Top Tech Issues

SonTek-SL: Using beam velocity data for QA/QC

The individual beam velocities should mirror each other (Figure 1) if the measurement site and installation complies with the specified requirements. It is expected that the beam velocities will not mirror each other exactly and it is acceptable if there are small variations between the two beams.

When using the beam velocities to analyze the data it is recommended that the data is evaluated over an extended period to identify a change in the data trend between the two beams. Evaluating a short period (couple of days) could be misleading. There are number of factors that can result in a difference between the beam velocities (Figure 2),

a) Vegetation or debris impacting the measurement volume of one of the beams,
b) Sediment deposition or sand bars moving downs stream that is impacting the measurement volume,
c) Algae or Biological growth on one of the transducers,
d) One beam interacting with water surface or channel bed
e) Fish presence in measurement volume.

It is important to note that Beam Velocities should not be used independently to review the data quality and that it should be used in conjunction with Standard Deviation of Velocity, Stage (Vertical Beam \ Pressure Sensor) versus Flow and BeamChecks data.

sl3g-beam-velocity-qa-qc-1.png

sl3g-beam-velocity-qa-qc-2.png

SL3G Standard Deviation of Velocity QA\QC

The standard deviation of the velocity between the two beams should be similar (Figure 1) for the entire profile if the measurement site and installation complies with the specified requirements. It is expected that there will be small variations in standard deviation between the two beams.

When using standard deviation of velocity to analyze data it is recommended that the data is evaluated over extended period to identify a change in the data trend between the two beams. There are number of factors that can result in a difference between the beam velocities (Figure 2),

a) Vegetation or debris impacting the cells located at the far end of the measurement volume,
b) Sediment deposition or sand bars moving downs stream that is impacting the cells located at the far end of the measurement volume,
c) One beam interacting with water surface or channel bed that is impacting the cells located at the far end of the measurement volume,
d) Fish presence in measurement volume.

It is important to note that Standard Deviation of Velocity should not be used independently to review the data quality and that it should be used in conjunction with Beam Velocities, Stage (Vertical Beam \ Pressure Sensor) versus Flow and BeamChecks data.

sl3g-standard-deviation-of-velocity-qa-qc-1.pngsl3g-standard-deviation-of-velocity-qa-qc-2.png