It looks like you are coming from United States, but the current site you have selected to visit is Guyana. Do you want to change site?

Yes, please! No, keep me on the current site

Wedeco Reuse UV Solution in Clovis, CA: City develops new sustainable water supply using “first of its kind” closed vessel UV installation

CLOVIS WATER REUSE FACILITY

USA

The city of Clovis in California constructs a new water reuse facility to reduce reliance on groundwater sources. The selected treatment process included a membrane bioreactor (MBR), ultraviolet (UV) disinfection system, and a two-stage solids reduction process, all with automated control and remote monitoring. At its maximum capacity, the Clovis Water Reuse Facility will be able to produce over two billion gallons (or 6,200 acre-feet or 7.7 billion liters) of water per year.

 

Download Case study