It looks like you are coming from United States, but the current site you have selected to visit is Belize. Do you want to change site?

Yes, please! No, keep me on the current site

Secure Connect API

The Secure Connect application programming interface (API) gives the external systems access to Secure Connect data. The following information is accessible through the APIs:

  • Alarms data
  • Live data
  • Station data
  • Device data
  • Customer data
  • User data

The Secure Connect APIs are only used to receive the data. The user cannot control the devices or edit data through the Secure Connect APIs by adding an external client.

Adding an external client

  1. Log in to Secure Connect.
  2. Go to Admin > Customers.
  3. Select a customer.
  4. Go to the External clients tab.
  5. Click the Add button.
  6. Enter a Name.
  7. Enter a Description.
    It is optional to write a description.
  8. Click Save.

An external client is created and the user gets a unique Auth0 Client ID and a one-time Auth0 Client secret. It is important to save the client secret as it is only displayed once. The client secret is required to access the Secure Connect REST APIs. If the user forgets the client secret, a new external client must be created.

 

API documentation

The Secure Connect API documentation is available in the Secure Connect application. To access the Secure Connect API documentation:

  1. Log in to the Secure Connect application.
  2. Click the profile icon in the upper right-hand corner.
  3. Click the External client resources.
  4. Click the API link to download the Secure Connect API YAML file.

The downloaded file contains the following information.

  • REST API paths
  • Request format
  • Response format
  • Schema information

To get the more information about the Secure Connect authentication mechanism and how to call the Secure Connect APIs, click the Installation Guide link on the External client resources. The downloaded file contains the following information:

  • Setting up an external client
  • Retrieving the JWT token for Authentication

Related FAQs

Many users have had similar questions about Analytics, Live Data, API and OPC UA Connector.