It looks like you are coming from United States, but the current site you have selected to visit is Belize. Do you want to change site?

Yes, please! No, keep me on the current site

TurboLIGHT Configuration

Modbus TCP connection

  1. Go to Control.
  2. Set MB_OFFSET_ADDR to 40 000.

The IP address of the blower must be the same in TurboLIGHT and Secure Connect. The IP address is shown in the Settings menu in TurboLIGHT.

Modbus RTU connection

  1. Go to Control.
  2. Set the Modbus address of the blower in the MB_SLAVE_NUM parameter.
  3. Go to Settings.
  4. Set the baud in the Modbus 485 parameter.

The Modbus address and baud must be the same in TurboLIGHT and Secure Connect.