It looks like you are coming from United States, but the current site you have selected to visit is Belize. Do you want to change site?

Yes, please! No, keep me on the current site

Illustrated Station Model

Get an illustrated model that shows the status of your station

The station model is an automatically created model that shows the machines and devices  connected to the station. The model also shows live data from the station. For example, the user can get an overview of the water level, how well the connected pumps are working.

It is possible to configure the model to show or hide different parts by using the configuration panel that can be accessed in the top right corner of the station model page. The station model is only available for stations with connected pumps.

Related FAQs

Many users have had similar questions about station management and station models.