It looks like you are coming from United States, but the current site you have selected to visit is Armenia. Do you want to change site?

Yes, please! No, keep me on the current site

Operation

Download the device documentation

The device documentation represents the device specification used in Secure Connect.

  1. Navigate and login into OPC UA Connector WebUI.
  2. In the top menu, click Documentation.
  3. Select document from the dropdown.
  4. Click the Open button to download the file

Enable anonymous OPC UA user access

Anonymous OPC UA User Access will allow OPC UA Read or Read/Write permissions for unauthenticated users.

  1. Navigate and log in to OPC UA Connector WebUI.
  2. In the top menu, select Users.
  3. Click the Anonymous access.
  4. Select Read or Read/Write to set permissions for anonymous access.
  5. Click the Save button.