See All QA Test - Product Family Page

XA QA Test Product Detail Page 1

Available for Rent
  • is the minimum order quantity for this product. Please check quantity and add to cart again.

Request Information

*  Required Field

This is the Short Description. This appears at the top and the first ~160 characters appear in cards on PFP pages. After the first three lines this area becomes expandable/collapsible. Recommended content: 1-2 Brief paragraphs introducing the product.

  • This is the Featured Bullet List- Only the first 5 lines will show (not 5 bullets)- Try to keep features concise- If they need to be longer, that's ok, just remember only the first five lines will be visible in this space- More than five lines and the area become expandable/collasible- This area should be simple bullets, no nesting- No text formatting (i.e. no bold/italicized/underlined text)- No closing punctuation- Sentence case

Featured Video Title - Watch me!

This is the long description. It will always start as a collapsed accordion with the option to expand.Lorem ipsum dolor sit amet, consectetur adipiscing elit. Duis nulla nunc, aliquam eget pretium vel, convallis sed dui. Aliquam interdum felis eget nibh tincidunt, quis vehicula turpis luctus. Nulla sit amet finibus leo, ac ultricies purus. Proin vel malesuada libero. Suspendisse placerat massa fermentum, fringilla mi sit amet, commodo turpis. Quisque non blandit arcu. Curabitur orci ligula, consectetur eu massa ac, laoreet vulputate velit. Sed nec metus nunc. Pellentesque cursus ut massa ac tempus. Donec vel lacus at felis tincidunt euismod eget vel tortor. Praesent consequat metus in interdum imperdiet. Nunc commodo convallis sagittis. Nullam ut efficitur neque, ut porttitor diam. Vivamus turpis tellus, maximus non magna et, dapibus pretium neque.Donec dapibus ligula eget sagittis accumsan. Praesent imperdiet est libero, tincidunt efficitur tortor maximus quis. Vestibulum ante ipsum primis in faucibus orci luctus et ultrices posuere cubilia curae; Ut feugiat arcu ut porta convallis. Vivamus porttitor condimentum odio. Integer tempor sollicitudin eleifend. Proin fermentum dolor in lacus tempor, id mollis ex faucibus. Sed fermentum aliquet nisi non molestie. Vestibulum tincidunt, orci sit amet laoreet tristique, sem nulla feugiat erat, at varius nulla libero vel ipsum. Pellentesque ut eleifend est. In ornare blandit erat, quis molestie magna viverra in. Nulla id feugiat purus. Nulla eget nibh a arcu egestas faucibus et a sem. Morbi vel posuere risus. Praesent luctus condimentum nulla, id finibus augue maximus mattis. Donec posuere dui sit amet nunc fermentum, eu porta ligula accumsan.Integer vehicula vitae felis sed fringilla. Integer convallis facilisis ex ut auctor. Vestibulum ut massa placerat, mattis lorem sed, hendrerit nibh. Fusce pharetra faucibus diam, a molestie nisl bibendum nec. Fusce aliquam eget odio sollicitudin congue. Vivamus id ligula faucibus, luctus lorem quis, interdum ex. Aliquam ornare molestie pharetra.

Do not use this space to list different variant features - use the Specifications area to display comparative specifications in a table format.

Feature 2 text Fusce sollicitudin quam sodales orci consequat, eget sollicitudin mi faucibus. Phasellus auctor posuere ante ut sodales. Vivamus erat dui, maximus nec eros vel, vestibulum finibus neque. In nec ultrices est. Nulla fermentum neque eu elit ultricies blandit. Donec non sapien a risus elementum malesuada. Aliquam iaculis interdum volutpat. Maecenas ac odio erat. Nunc dictum magna eget magna scelerisque posuere.##### Caption is written using H5

Specifications

Cards Block title (optional, sentence case)

Cards Block description (optional, sentence case) - The following page types can be pulled into this area: Market/Application, Resource, Product, Brand, Case Study, Call to Action. Custom cards can also be created using an image, Title, text and optional link. Maximum 4 cards per row. Less than 4 will fill the width of the space. Can select how many cards to show initially, either 4, 8 or All. Blocks have a charter limit of 148 characters (no spaces)/175 characters (with spaces). If you go over that then if will cut it off with ...

  • Upper Gwynedd Township, PA. Wastewater Treatment Facility case study image. Image depicts water dripping off a leaf and into a body of water

    Aerobic system to provide sustainable treatment solution

    ​Evoqua Water Technologies has been selected by Carolina Water Service, Inc. of North Carolina, through its sales partner Premier Water, to design, manufacture and install a new wastewater treatment system located in the gated golf course community of Connestee Falls, N.C. The plant was designed to be sustainable, with a focus on increasing the plant's efficiency and extending its useful life.

  • Hot Springs: combating aging infrastructure challenges with Xylem digital solutions

    Many water pipelines in the United States were installed in the early to mid-20th Century, with some systems still relying on cast-iron pipes more than 100 years old. Aging infrastructure stands as a critical challenge in the water sector for utilities across the nation, posing significant threats to the reliability and safety of water systems.

  • From digital twin to decision intelligence

    This guide aims to help utilities answer three key questions: What role can digital twin technology play in optimizing operations? How can utilities apply this technology to maximum effect? What can we learn from those utilities leading the way?

  • City of Tulare Celebrates 25 Years of Converting Waste-to-​Energy case study image

    City of Tulare celebrates 25 years of converting waste-to-​energy

    The City of Tulare, located in California’s world renowned San Joaquin Valley, is known for its rich agricultural and dairy industries. Tulare is home to six large-scale cheese and dairy producers. Like many municipalities, the city is challenged to meet industrial requirements at a reasonable cost while maintaining harmonious relationships with the surrounding community.

  • Cover Helps Community Control Odors from Wastewater Treatment case study image

    Cover helps community control odors from wastewater treatment

    When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.

  • Covers Help Keep Kamloops Beautiful case study image

    Covers help keep Kamloops beautiful

    The City of Kamloops is located in the interior of British Columbia, Canada’s westernmost province. Situated along the scenic Thompson River, the city’s wastewater treatment facility currently serves a population of over 80,000 people and treats a daily flow of 40,000 m³ (10 mgd), a number which would soon increase to 60,000 m³ (16 mgd).