It looks like you are coming from United States, but the current site you have selected to visit is Equatorial Guinea. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Xylem’s new adaptable wastewater mixer delivers next-level mixing efficiency

abril 11, 2018

RYE BROOK, New York, April 11, 2018 – Leading global water technology company,Xylem Inc. (NYSE: XYL) has launched a compact submersible wastewater mixer featuring easily adaptable output capabilities and delivering energy savings of approximately 50 percent. Xylem’s new Flygt 4220 mixer enhances the resilience and sustainability of wastewater treatment plants, enabling operators to easily manage changing mixing conditions by simply adjusting the mixer output. As the Flygt 4220 can be controlled to deliver only the output required, a plant’s energy consumption can be significantly reduced.

“Plant operators are looking for mixer technology that enables them to increase operational efficiency, improve performance based on their specific system demands, and provide real-time data to extend product lifecycle and reduce downtime and maintenance costs,” said Johan Tegstam, Director, Product Management for Xylem. “The beauty of our new Flygt 4220 mixer lies in its adaptability. Plant operators can easily modify the mixer output, via a tank-side control panel, a programmable controller or plant-wide control system, to match current mixing needs. This functionality dramatically reduces energy consumption compared to traditional fixed output mixers, significantly improves process productivity and futureproofs a facility’s mixing efficiency. We’ve designed the Flygt 4220 mixer to deliver comprehensive information about the mixer’s performance and status, including speed, power, alarms, running time and energy consumption. The mixer features a number of auto-correction functions, including overload control to protect the equipment and secure process results.”

Wastewater mixing is not a static process, as mixing requirements will vary over time depending ona range of factors includingflow rates, oxygen demand, and seasonal variations. Conventional mixers operate at a fixed output which often results in wasted energy, unnecessary wear and increased maintenance due to inefficient operation of the mixer.

“The Flygt 4220 mixer fits all common installation systems and is ideal for retrofits, slotting easily into an existing installation. It is a great choice for municipal or industrial wastewater or sludge mixing applications,” concluded Tegstam.

The Flygt 4220 mixer is based on Xylem’s Flygt Dirigo platform of integrated power electronics, including an IE4 super premium efficiency motor that delivers market-leading efficiency, and is available in 1.5, two, three and four horsepower versions.

The mixer’s capacity to deliver a wide range of duty points – unlike the fixed output generated by single-speed mixers – enables a single Flygt 4220 to replace multiple conventional mixers and will require fewer complete mixers and parts in stock. Flygt 4220 also offers lower investment for rebuild or replacement as it can be redeployed across different tanks and applications.

The Flygt 4220 joins the larger Flygt 4320 mixer, launched in 2015, as part of Xylem’s range of adaptive wastewater mixers.

About Xylem

Xylem (XYL) is a leading global water technology company committed to developing innovative technology solutions to the world’s water challenges. The Company’s products and services move, treat, analyze, monitor and return water to the environment in public utility, industrial, residential and commercial building services settings. Xylem also provides a leading portfolio of smart metering, network technologies and advanced infrastructure analytics solutions for water, electric and gas utilities. The Company’s more than 16,500 employees bring broad applications expertise with a strong focus on identifying comprehensive, sustainable solutions. Headquartered in Rye Brook, New York with 2017 revenue of $4.7 billion, Xylem does business in more than 150 countries through a number of market-leading product brands. 

The name Xylem is derived from classical Greek and is the tissue that transports water in plants, highlighting the engineering efficiency of our water-centric business by linking it with the best water transportation of all – that which occurs in nature. For more information, please visit us at www.xylem.com.

Xylem Inc.

Media
Amanda Holloway
Amanda.holloway@xyleminc.com
+1 (224) 500-0742

Xylem