It looks like you are coming from United States, but the current site you have selected to visit is South Korea. Do you want to change sites?

Yes, please. No. Keep me on the current site.

EnviroMix eases maintenance demands and delivers energy savings with BioCycle-D process

Wastewater Reclamation Facility in Highland, Illinois 

Wastewater Reclamation Facility in Highland, Illinois - fine bubble aeration
The fine bubble aeration system provides process oxygen while BioMix provides independent mixing. 

Founded in 1831, Highland, Illinois, is one of the oldest Swiss settlements in the United States. Located 35 miles east of St. Louis, Highland is home to a population of about 10,000 residents.

In 2020, the City of Highland extensively upgraded their water reclamation facility (WRF), which had last been upgraded in 1997. The scope of the project consisted of new headworks, secondary clarification, aerobic digestion, sludge holding, and sludge dewatering. Replacing equipment that had reached the end of its operating life, the upgrade was designed to ease operation and maintenance demands and improve energy efficiency, allowing the plant to meet current and future permitted effluent limits for nitrogen and phosphorus.  

Challenge

Previously, the aerobic digester was aerated and mixed via inefficient coarse bubble diffused aeration with air lift pumps that transferred sludge between cells; the digested sludge holding tank was mixed with an inefficient pump mix system. Highland’s supervisor Bill Zimmer commented, “Our old digester was labor intensive… we had to check it constantly, and we were wasting a lot of energy.”

Solution

EnviroMix’s energy-efficient BioCycle-D Optimized Aerobic Digestion Process was selected as a key treatment technology to replace the inefficient, conventional solutions in the aerobic digester and the sludge holding tank. After visiting other installations in Illinois, Highland’s staff were impressed by BioCycle-D’s outstanding operation, performance, and energy savings.  

BioCycle-D is designed by right-sizing the diffused aeration system to satisfy process oxygen demand and applying energy efficient mixing through a BioMix Compressed Gas Mixing System. The process decouples aeration from mixing, facilitating independent control over oxygen delivery and mixing, thus preventing over-aeration and wasted energy.  

Through aerobic and anoxic cycling, BioCycle-D maximizes volatile sludge destruction, minimizes energy consumption, recovers alkalinity, and provides denitrification, significantly reducing nutrient recycle to the main treatment process. The plant is able to operate the system as digesters in parallel or series depending on treatment demands. 

Wastewater Reclamation Facility in Highland, Illinois - rotary screw compressors for BioMix
Rotary screw compressors provide high pressure mixing air to the BioMix system. 

Results

Decoupling aeration from mixing provides the Highland WRF with more than 75% energy savings at design loading and even greater savings at the reduced current sludge loading, resulting in annual operational savings of more than $200,000. 
“Since the upgrade — even though we’ve added three blowers and two compressors and doubled our capacity — in reality, we’re using less energy than we were,” stated Zimmer. 

Wastewater Reclamation Facility in Highland, Illinois - hybrid blowers for fine bubble aeration
Hybrid blowers provide air to the fine bubble aeration system. 

0.12 HP/1,000 Cubic FT Mixing Efficiency

75% energy savings vs. diffused aeration

“What I like most about BioCycle-D is the functionality — the automatic operation of the decanting is very nice. everything just flows now and it’s not so labor intensive.”
Bill Zimmer, Highland WRF Supervisor