It looks like you are coming from United States, but the current site you have selected to visit is South Africa. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

The world’s first wastewater pumping system with integrated intelligence

Xylem has developed a smart wastewater pumping system that senses the operating conditions of its environment, adapts its performance in real time and provides feedback to pumping station operators. The new Flygt Concertor is the world’s first wastewater pumping system with integrated intelligence. Find out about its unprecedented flexibility and reduced cost of ownership.

Fields tests conducted around the world have proven Flygt Concertor’s significant improvements in wastewater pumping. These include:

– Energy savings of up to 70% compared to conventional pumping system

– Reduced inventory by up to 80% due to flexible performance

– Clog-free pumping operation and clean wet wells saving up to 80% in vacuum cleaning costs

– A compact design, reducing cabinet size by up to 50%.

Flygt Concertor represents a step-change in sustainable wastewater management solutions, with unparalleled pumping efficiency and reliability as well as a lower overall cost of ownership,” said Tomas Brannemo, President of Xylem’s Transport business. “It significantly advances the wastewater pumping sector by simplifying the entire pumping process from selection, installation, commissioning and monitoring with the added bonus of a smaller footprint. Flygt Concertor is a real problem solver, developed in close collaboration with our customers around the world.”

Designed to work in harmony

The name Concertor is derived from the Latin concentare, meaning “working together to orchestrate harmony”. Flygt Concertor is suitable for use with wastewater pumps in the range of 2.2 to 7.3 kilowatts (kW) and has a system design that combines IE4 motor efficiency, N-hydraulics, integrated power electronics and intelligent controls. All these features are designed to work in harmony with each other, which results in optimal pumping performance at the lowest cost of ownership.

Flygt Concertor’s flexible performance represents a significant change in how pumping systems will be selected and managed in order to accommodate different flow rates. In contrast to the fixed performance curves of conventional pumps, Flygt Concertor offers a wide performance field from which to choose the right operating point. This makes selection extremely simple, facilitates performance fine-tuning and, as a consequence, significantly reduces inventory.

Eliminates clogging, built-in cleaning

Concertor features a built-in sump and pipe-cleaning features – a first for a wastewater pumping system. Extensive trials show that these features, together with a second generation of Flygt’s patented Adaptive N-technology and an integrated pump-cleaning function, minimize vacuum cleaning costs. When tested at a pumping station in Heathrow Airport, the combined performance of these functionalities successfully eliminated regular clogging issues and kept the sump clean.

“Since installing Concertor we have had absolutely no clogging and the sump remains clean,” said Ian Jolly, Systems Specialist for Water, Heathrow Airport Water Services Department. “As well as peace of mind, the cost savings are approximately 87.5 percent of the annual costs in cleaning and servicing.”

Meeting the future challenges of the industry

Flygt Concertor provides customers with the technology needed to increase the sustainability of their wastewater management operations.

“The development of Flygt Concertor is another demonstration of Xylem’s commitment to develop innovative and integrated designs that meet the future challenges of the industry,” said Christian Wiklund, Vice-President, Director of Product Development. “We know that the answer to these challenges is not more components and complexity, but rather sophisticated, user-friendly pumping systems like Concertor.”

Concertor shares a rich heritage with other Flygt innovations, such as the world’s first submersible wastewater pump in mid-1950, a revolutionary self-cleaning hydraulic design in 1997, and an intelligent wastewater control in 2011.

“We are determined to push the limits of technology to create the highest quality, most reliable and sustainable wastewater pumping systems on the market. Flygt Concertor is the realization of that ambition,” said Peter Lewington, Director Wastewater Pumping. “It is our customers’ needs that drive us, and at the end of the day, their peace of mind is the true measure of our success.”

by Chad Henderson