Digital suspended solids sensor with ultrasonic cleaning, connectable to the IQ SENSOR NET
ViSolid®: Optical sensors for the in-situ use to measure suspended solids via scattered light and direct back-scattering with ultrasonic cleaning system:
The ultrasonic cleaning system ensures the low-maintenance and continuously reliable measuring operation of the sensors, which are therefore very suited for extreme applications, such as wastewater treatment plants.
With higher particle concentrations, the procedures of turbidity measurement are only suitable in some cases; here, you will need special measuring techniques to determine the concentration. WTW uses two procedures, which are used depending on the suspended solids concentration: With low concentrations, a scattered light measurement is used; for higher concentrations, the direct back-scattering yields optimal results.
ViSolid® 700 IQ (600012):
ViSolid® 700 IQ SW (600013):
* SW: Sensor as sea water model (with plastic arming (POM))