Digital pH/ORP armature to be used with electrodes, connectable to the IQ SENSOR NET
SensoLyt® 700 IQ – digital pH/ORP armature with integrated preamplifier and temperature sensor as well as lightning protection to be connected to IQ Sensor Net:
By storing calibration values within the sensor, a "pre-calibrated pH-measurement" can be generated. Due to our quick-lock, the sensor can be disconnected and – after laboratory calibration – re-connected at the site easily. Inconvenient calibrations in the field under adverse conditions can be completely eliminated if there is an IQ connection in the lab.
A special switch also allows automatic monitoring for glass breakage. The required replacement of the SensoLyt® electrode is quick and uncomplicated.
SensoLyt® 700 IQ (109170):
SensoLyt® 700 IQ SW (109171):
SensoLyt® 700 IQ/SET (109173):
SensoLyt® 700 IQ/SET1 (109174):
* SW: Sensor as sea water model (with plastic arming (POM))