Adapter installed at the end of the suction hose
Adapter, female 3/4inch-14BSPP to barbed 3/8 inch IDThis adapter is installed at the end of the suction hose and allows for connection of the suction hose to the intermediate tube.All YSI suction hoses have the 630127 adapter pre-installed. If not using a YSI suction hose, ensure the suction hose being used has a ¾ inch-14BSPP connection. The ¾ inch-14BSPP female adapter (630127) can be installed on the suction hose if it does not have a ¾ inch-14BSPP connection.Please see the ProSample Ordering Guide if ordering a complete system, or contact us if you have any questions.